Cancel
Showing results for 
Search instead for 
Did you mean: 

Custom toolbar

Phenom
Phenom

NX11 with TC 11

 

I've sccumulated a few journals over time, and as useful as they are, trying to get other users to use them, or even remember they exist is a challenge.  So, I'd like to create a new tab on the ribbon bar, which would be company specific.

 

I think I've figured out the syntax to create the actions, and buttons are just a function of taking the time to make them.  My question is, what variables do I need to set, and where do I locate the .tbr file?

 

Any tutorials on this out there?

-Dave
NX 11 | Teamcenter 11 | Windows 8.1
3 REPLIES

Re: Custom toolbar

Esteemed Contributor
Esteemed Contributor

Go to this document in UGanswer

https://solutions.industrysoftware.automation.siemens.com/docs/newsletter/NX-Ribbon-Customization-an...

 

If that link doesn't work, try searching on "NX_Ribbon-Customization_and_Transition"

 

Lots of cool stuff - ribbons specific to each application, etc.

Ken

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP5 + patch/TC11.2
I'd rather be e-steemed than e-diseaseled


Re: Custom toolbar

Esteemed Contributor
Esteemed Contributor

and (if you don't have it already) if you use Notepad++ to edit text files, search this forum for "Notepad++ customizations for NX"

 

There's languages defined for each of the ribbon/toolbar file types (plus lots of other NX related file types)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP5 + patch/TC11.2
I'd rather be e-steemed than e-diseaseled


Re: Custom toolbar

Legend
Legend

Here is the word document as a pdf.

 

Frank Swinkels