Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Customer Default for different user

Phenom
Phenom

Hi,

we share customer default for our 30 NX seats. One user doesn't like the 'Pack components' setting for assembly loading.

Annotation.png

How can I set for only this user, only this modified setting?

Thank you..
Using NX1880 and RuleDesigner PDM

Built-in functions for converting units of measure

3 REPLIES 3

Re: Customer Default for different user

Siemens Phenom Siemens Phenom
Siemens Phenom

Customer defaults can be applied at 3 levels Site, Group and User.

 

You can define "common" defaults at the site or group level. Users could pick their own settings at the user level.

 

Note that each default can be locked at the site or group level if you want to prevent a user from changing them at the user level.

 

See Levels of customer defaults in the online documentation

Re: Customer Default for different user

Phenom
Phenom

Hi @JimB,

it's all clear, but I have some questions. Can I have a different customer defaults for each NX user?

For example, a customer defaults for Bill, a customer defaults for Alex, etc?

How can I protect the customer defaults site by users modifications?

Actually, the shared folder that contains all NX setting and reuse library is open for all technician.

Thank you..
Using NX1880 and RuleDesigner PDM

Built-in functions for converting units of measure

Re: Customer Default for different user

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Every user can still have their own customer defaults.

I'm not sure exactly what controls what, but at our site we define the ENV variable UGII_LOCAL_USER_DEFAULTS to point to the user-level customer default file.

 

If you want to "lcok down" the site level defaults:

1) Set the Windows (OS) permissions on the folder so only the correct people have write access

This will prevent random users from changing the site level defaults

2) If you want to prevent users from changing a particular setting (over-riding the site level setting with their user level one) you can "lock" the site level setting.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled