Showing results for 
Search instead for 
Do you mean 
Reply

Cut specific teamcenter-relation with NXOpen?

Hello,

 

Is it possible to cut a specific non-master part (PDF) in teamcenter with NXOpen?

 

Actual situation:
After a save operation in NX we will create a PDF automatically in teamcenter (PrintPDFBuilder)

 

Problem:
The name of this PDF is: ItemID_ItemRevID_ObjectName
So if the revision will be renamed NX will create a second PDF and doesn't overwrite the existing one.

Work-around:
1) Before the program creates the new PDF it should cut the old PDF, but I don't know if it is possible to cut relations in teamcenter with NXOpen.

2) Otherwise I must create a post-action in teamcenter that removes the old PDF

 

Thanks,

3 REPLIES

Re: Cut specific teamcenter-relation with NXOpen?

Hi,

You can't do it with NXOpen but you can call SOA  methods to do it from your NXOpen code. Maybe better solution than defining a postaction.

Regards,

Xtof

Re: Cut specific teamcenter-relation with NXOpen?

Thank you for this information.
Is there an sample code how can I call SOA methods in NXOpen?
Thanks,

Re: Cut specific teamcenter-relation with NXOpen?

 

Yes, we distribute an example with NX.  Have a look in this folder, wherever you have NX installed:

 

...\UGOPEN\SampleNXOpenApplications\C++\SOAConnectionExample

 

Note that it will make a new connection to the database.  Be sure to have a close look at the "SOAConnectionExample_ReadMe.txt" file in that folder.