Cancel
Showing results for 
Search instead for 
Did you mean: 

Datum CSYS User Attributes

Experimenter
Experimenter

Why am I not able to read the user attributes assigned to a Datum CSYS? Here is a snippet of code in which I loop through a work part's features looking for a specific name, then I try to get the attributes.

 

For Each temp As Features.Feature In workPart.Features
                If temp.Name = nameToFind Then
                    test1 = temp
                    found1 = True
                    Exit For
                End If
            Next

            If found1 Then

                Dim myObject() As NXOpen.NXObject = test1.GetEntities()

                myAttributes = test1.GetUserAttributes()

 

This approach works great for Points but doesn’t work with Datum CSYS. I think this may be a problem on the NX side??? Here is a comparison of the NX generated information between a Point and Datum CSYS with user attributes.

 

Point – User Attributes (note, the feature attributes are clearly defined)

point.png

 

Datum CSYS – User Attributes (note, feature attributes are listed but not clearly defined with a title compared to the above)

csys.png

 

When I run the code above, I am able to pull the user attributes out of Point but not Datum CSYS. The above seems to be the only logical reason why to me…

 

6 REPLIES

Re: Datum CSYS User Attributes

Esteemed Contributor
Esteemed Contributor

Check the object type & subtype of what you find.

 

Actually, first thing I'd do is remove the "exit for", put a counter in & see how many objects match the name (and what each object type & subtype are).

 

Could be you're not finding what you think you are looking for...

 

Ken

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP5 + patch/TC11.2
I'd rather be e-steemed than e-diseaseled


Re: Datum CSYS User Attributes

Honored Contributor
Honored Contributor

Does your code generate the attribute report? If so, could you show the code that writes to the listing window (or other location)? It doesn't seem to be included in the code snippet that was posted.

 

Were the attributes assigned to the datum csys feature or to the datum csys object itself? Objects and features can each have their own set of independent attributes. Make sure that you are applying them to and querying them from the correct type.

Re: Datum CSYS User Attributes

Experimenter
Experimenter

I did as you recommended and am selecting the correct feature based on the feedback from the counter.

Re: Datum CSYS User Attributes

Experimenter
Experimenter

I list out the name and feature name in the listing window after I recieve a name match as you can see below. I repeated portions of the snippet above so you can follow the flow of the code more easily. The code does not generate the attribute report but as I debug and run through the loop I note the the variable attributeLength does not get populated as it passes through the Datum CSYS.

 

I believe they were assigned to the feature as it was performed by right clicking and selecting properties from the feature listed in the Part Navigator. Forgive me I am new to NX, but how can one tell the difference between a feature and an object?

 

I have attached the Information on the feature that is found when right clicking on the feature in the Part Navigator and selecting Information.

 

For Each temp As Features.Feature In workPart.Features
                If temp.Name = nameToFind Then
                    test1 = temp
                    found1 = True
                    Exit For
                End If
            Next

            If found1 Then

                Dim myObject() As NXOpen.NXObject = test1.GetEntities()

                myAttributes = Nothing
                attributeLength = Nothing
                myAttributes = test1.GetUserAttributes()
                attributeLength = myAttributes.Length

                For Each obj As NXObject In myObject
                    If TypeOf (obj) Is NXOpen.Point Then
                        Dim feat As NXOpen.Point = obj
                        Dim myCoordfeat As Point3d
                        myCoordfeat = feat.Coordinates
                        lw.WriteFullline(test1.Name & "-" & test1.GetFeatureName & ": " & myCoordfeat.ToString)

 

Re: Datum CSYS User Attributes

Experimenter
Experimenter

I figured out the issue, thanks @cowski1, your post was the key. When setting attributes on a Datum CSYS, in the Property dialogue box you can select to apply to the object or the feature as shown below. Changed it to apply to the feature and code works as intended.

 

attribute assignment.png

Re: Datum CSYS User Attributes

Honored Contributor
Honored Contributor

If you apply the attributes in interactive NX, make sure that you check the Context -> apply to option. I'm running NX 9, when I right click on a datum csys, it seems to default to object rather than feature. If your code isn't reporting attributes on a particular datum csys feature, it would indicate to me that perhaps the properties were applied to the object rather than the feature. You can check this by right clicking on the datum csys and toggling between the feature and object attributes.

 

csys_props.png

 

 

Edit: glad you got it working...