Cancel
Showing results for 
Search instead for 
Did you mean: 

Delet condemned objects

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi,

 

I am trying to delet a coordinate system object of type 45 and subtype 0 see diagram below

(uf_object_types.h  #define UF_coordinate_system_type                45).

 

But the problem is that the object is by creation in "condemned" state and using UF_OBJ_delete_object() does not seem to work on this type of objects. I want delet only specific objects and not all condemned obects in the work part.

 

I also tried some solution in from Journaling, such as

 

  int nErrs1 = theSession->UpdateManager()->AddToDeleteList(m_CSys);
  notifyOnDelete = theSession->Preferences()->Modeling()->NotifyOnDelete();
  nErrs1 = theSession->UpdateManager()->DoUpdate(markId);

 

but that only works in Journaling mode and in written code application this also does not delet object with condemned status.

 

Is there any option to delete selected condemned objects?

 

The Coordinate system object of type 45The Coordinate system object of type 45

 

Best regards

 

Riaz Ur-Rehman

Aixpath GmbH

 

 

2 REPLIES

Re: Delet condemned objects

Phenom
Phenom

I think you may not be able to delete condemned objects selectively. but can delete all the condemned objects in the part with UF_SO_delete_non_deletables..

 

Suresh

Re: Delet condemned objects

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi, Tanks a lot for the inputs. Yes, the statement is known to me. However, as I said, I need to delet only specific objects and not all. So this would not work in this case.