Cancel
Showing results for 
Search instead for 
Did you mean: 

Determining reference set used to perform boolean

Innovator
Innovator

 

If you have a linked body in a component, how do you determine which reference set the linked body is using? We can determine the body in the owning part, but not the reference set.

3 REPLIES

Re: Determining reference set used to perform boolean

Valued Contributor
Valued Contributor

Can't you cycle through the ref sets in the owning part and check if the body you've identified belongs to it's object list?

Re: Determining reference set used to perform boolean

Esteemed Contributor
Esteemed Contributor

Note a body may belong to more than 1 reference set (actually, if it is in anything other than "Entire Part", then "by definition" it is in more than 1 ref set).

 

Not that this gets you closer to your answer.

 

You may have to think of it in a different way, e.g.:

Is there a way to query a component (part) which of its ref sets is being used in the assembly?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP5 + patch/TC11.2
I'd rather be e-steemed than e-diseaseled


Re: Determining reference set used to perform boolean

Innovator
Innovator
**bleep** that's a good point. Haha
Thank you.