Cancel
Showing results for 
Search instead for 
Did you mean: 

Disable feature error messages

Pioneer
Pioneer

Hi,

I need to disable in visual basic the warning message about problems with some feature.

In my case I need to disable the error message on a boolean operation to avoid to click "OK" on the pop-up as you can see in the attached image.

 

Thanks for your help

2 REPLIES 2

Re: Disable feature error messages

Siemens Phenom Siemens Phenom
Siemens Phenom

Any message box like this that is displayed when running an NX Open application is a bug. Message dialogs requiring user action to continue should only be displayed in an interactive session. When an NX open application is running, the message should be suppressed and a corresponding exception should be thrown that the NX Open code can catch.

 

Please file a PR on this issue through GTAC.

Highlighted

Re: Disable feature error messages

Pioneer
Pioneer

Hi Jim, sorry but I didn't catch your answer.

 

Could you give me some clarifications.

 

Thanks 

 

Luigi