Cancel
Showing results for 
Search instead for 
Did you mean: 

Does NX10 supports functions in Open C

Pioneer
Pioneer

Hi, 

    Recently I wrote an application using Open C library, it work well on NX9, however it doesn't work on NX10. The function which doesn't work is UF_LAYER_create_category, when I want to create a category with layer from 1 to 100, it can work on NX9, however on NX10, it just create a category with the current layer number.

Any suggestions? Thank you!

2 REPLIES

Re: Does NX10 supports functions in Open C

Esteemed Contributor
Esteemed Contributor

Did you re-comiple/link the DLL with NX10?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP5 + patch/TC11.2
I'd rather be e-steemed than e-diseaseled


Re: Does NX10 supports functions in Open C

Phenom
Phenom

Yes, try to recompile as Ken suggested.  I tried to create layer category and seems to work fine for me.

Suresh