Cancel
Showing results for 
Search instead for 
Did you mean: 

Editing a spreadsheet controlled Tabular Note

Pioneer
Pioneer

Is it possible to edit the contents of a cell in a spreadsheet controlled tabular note? I can read and write to a non spreadsheet controlled tab note, but I am only able to read from one that is spreadsheet controlled. The code does not error when "writing", it just does not change the text.

1 REPLY

Re: Editing a spreadsheet controlled Tabular Note

Pioneer
Pioneer

Unfortunately this doesn't appear possible at the current time. This IR was converted into an enhancement request (ER) on 20-OCT-2015 and is now referenced as ER Number 7540975. It is OPEN for review at this time.

 

See the discussion on nxjournaling.com below. for more info.

 

http://nxjournaling.com/content/editing-spreadsheet-controlled-tabular-note