Cancel
Showing results for 
Search instead for 
Did you mean: 

Exploded Components in Drafting View

Valued Contributor
Valued Contributor

 Hello Everyone,

 

Whenever I query a Drafting View, AskVisibleObject API will return me components, Solidbodys,Draftingcurves and etc. To my surprise now I see Exploded Components instead of Components.

 

exploded component.JPG

 

Can someone help me to understand,

1. The scenario when do I get exploded components in a drafting view?

2. Is there any settings which should be turned ON/OFF to get the visible objects in a view as Component instead of Exploded Component?

 

Thanks,

Shanmugam.K

2 REPLIES 2

Re: Exploded Components in Drafting View

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

What version of NX are you using?

The view that you queried: does it have an explosion applied to it?

Re: Exploded Components in Drafting View

Valued Contributor
Valued Contributor

Hi Cowski,

 

I am using NX11.0.2.7. 

 

No, the view didnot have any explosion applied. I also tried delete explosion using Assemblies --> Exploded Views --> Delete Explosion option, but I was getting a message there is no explosion.

 

Thanks & Regards,

Shanmugam Sundaram.K