Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Export assembly to Excel with picture

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Try it again (new version published to same link as previous post).

Re: Export assembly to Excel with picture

Experimenter
Experimenter

Hello All 

 

Please help me I had problem when i try this journal

 

Problem.JPG

Re: Export assembly to Excel with picture

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Upgrade to NX 8 or later; that journal won't work with NX 5.

Re: Export assembly to Excel with picture

Creator
Creator

Hi. I am using Team Center (PLM) same code not working for me.

i want to export NX bom to excel with pictures.

can u please provide the journal code?

 

Re: Export assembly to Excel with picture

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I don't suggest using the code that was posted in this thread as it was customized for cubalibre's specific needs. Instead, start with this code; it is a more generic version that should work with native NX or with teamcenter (it assumes you are using the default english TC attribute names).

 

Credit for the journal code goes to Ian Eldred.

Re: Export assembly to Excel with picture

Phenom
Phenom

Hi @cowski1,

the journal is very used and liked. I've two problems :

1) It's seams that if the Excel file is sent to other, images aren't visible. Aren't embedded in the Excel file ? If not, can be embedded ?

2) We have some assembly, where some parts aren't loaded cause reference set and in this case, the journal finish to cross the assembly. Can the journl be modified to bypass not loaded parts ?

Thank you...

Using NX1867
RuleDesigner PDM

Re: Export assembly to Excel with picture

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

All credit for the code goes to Ian Eldred. He wrote it while working in an NX/TC environment. I made a few minor tweaks for native NX users; beyond that, I have no plans to maintain the code or add new features.

Re: Export assembly to Excel with picture

Experimenter
Experimenter

Hi,

Can anybody send me code to export BOM with pictures to excell ?

I have NX10 native without TC. Unfortunatelly downloaded macros are freazing my station for hours without success Smiley Sad

Re: Export assembly to Excel with picture

Experimenter
Experimenter

Hello, i know this post is very old, but I wonder if you could share that code again, as the shared link seems to be down.

I've been trying to run the code, but the images don't appear on the generated Excel file. The screenshots are taken, as they appear on the specified folder path.

I'm running Native NX11 and Excel 2013.

 

Thank you very much in advance.

Julien