Cancel
Showing results for 
Search instead for 
Did you mean: 

Export custom "toolbar" in NX9 to use it in NX10

Phenom
Phenom

To all

 

just did the updgrad to NX10. Is there a way of exporting a custom toolbar (My Items/My User Commands) from NX9 to import in NX10? Or do I have to re-create everyting from sractch!

 

Thanks

Regards

Production: NX9.0.3.4, NX10.0.2.6
Development: VB.NET (amateur level !)
12 REPLIES

Re: Export custom "toolbar" in NX9 to use it in NX10

Esteemed Contributor
Esteemed Contributor

Anything you have done inside of NX, to customize the tool bars or ribbons, must be recreated from scratch.

If you like to have this available separately, you will have to create a tool bar file using NX menuscript.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.0, FBM, MRL 3.1.4 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 10.1
Development: VB.NET, Tcl/Tk    Testing: NX12.0

How to Get the Most from Your Signature in the Community

Re: Export custom "toolbar" in NX9 to use it in NX10

Phenom
Phenom

Thanks . Fantastic, more time spent waffing about with NX.....

I did have a look at a .tbr file but If my memory serves me right one cn only call a .dll file. Which I cannot create because of IT security

 

Production: NX9.0.3.4, NX10.0.2.6
Development: VB.NET (amateur level !)

Re: Export custom "toolbar" in NX9 to use it in NX10

Honored Contributor
Honored Contributor

You can invoke uncompiled journals using toolbar (or ribbon) files and menuscript.

Re: Export custom "toolbar" in NX9 to use it in NX10

Phenom
Phenom

I'll have to have a look at that again then.

Production: NX9.0.3.4, NX10.0.2.6
Development: VB.NET (amateur level !)

Re: Export custom "toolbar" in NX9 to use it in NX10

If you use file-based customization, then you can easily add your NX 9 toolbar to your NX 10 ribbon. 

 

If you don’t have it, there is a very good document on customizing the ribbon, and transitioning toolbars:  https://download.industrysoftware.automation.siemens.com/unigraphics/ugdoc/nx9/nx-9.0.0/NX_Ribbon-Cu...

 

Mark Rief
Retired Siemens

Re: Export custom "toolbar" in NX9 to use it in NX10

Phenom
Phenom

I cannot download the file despite being logged in!

Production: NX9.0.3.4, NX10.0.2.6
Development: VB.NET (amateur level !)

Re: Export custom "toolbar" in NX9 to use it in NX10

Phenom
Phenom

It is in the downloads section of GTAC and requires a webkey login.

Community login will not work.

Re: Export custom "toolbar" in NX9 to use it in NX10

Phenom
Phenom

got the doc. Thanks

Production: NX9.0.3.4, NX10.0.2.6
Development: VB.NET (amateur level !)

Re: Export custom "toolbar" in NX9 to use it in NX10

Siemens Phenom Siemens Phenom
Siemens Phenom

Interactive customizations are stored in the user.mtx file located in:

 

C:\Users\<username>\AppData\Local\Siemens\NX##

 

There's not a supported way of migrating these. You could try simply copying the file from the NXN90 folder to NXN100. If not, it's just XML, so you may be able to use differencing tools, etc. to figure out what to strip out and copy to the new version.

Long term, you should use toolbar/menu/ribbontab files to make "permanent" UI customizations.