Cancel
Showing results for 
Search instead for 
Did you mean: 

Export objects to a separate part

Creator
Creator

Hello everyone!

 

Is there is a way to export the selected objects to a separate file?

Currently i'm using workPart.SaveAs("..."), but it doesn't allow to return to the previous undo state. Thanks!

 

Regards.

3 REPLIES

Re: Export objects to a separate part

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The following thread has some code that might get you started:

http://www.eng-tips.com/viewthread.cfm?qid=336277

Re: Export objects to a separate part

Creator
Creator
Thanks cowski1!

Is it also possible to export only the selected faces to a separate file?

Re: Export objects to a separate part

Siemens Phenom Siemens Phenom
Siemens Phenom

 

Faces need to belong to a body, so you can't export them as stand-alone entities.  But you could extract a sheet body for each face, and then you could export those sheet bodies.