Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Export text from the Operation's information window

Valued Contributor
Valued Contributor

Hey everyone,

 

I'm looking for way to be able to reach to the text of the operation's information window.

I want to export specific sections from it. Is it possible?

 

Best regards,

Tom.

3 REPLIES

Re: Export text from the Operation's information window

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Check the ListingWindow methods for those related to file actions.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Export text from the Operation's information window

Genius
Genius

Hello Tom!

 

You can pipe the information window to an external file using something like that (e.g. in C#):

1) Session curSession = Session.GetSession();
2) ListingWindow curLw = curSession.ListingWindow;
3) String curPath = @"C:\myFile.txt";
4) curLw.SelectDevice(ListingWindow.DeviceType.File, curPath);
5) curLw.Information.DisplayObjectsDetails(someObjects);
6) curLw.SelectDevice(ListingWindow.DeviceType.Window,"");

  This is a simple example for an output pipe:

Line 1-3: Some definition stuff

Line 4: Now, the output of the ListingWindow will go to a specific file (myFile.txt)

Line 5: Make some output in the ListingWindow

Line 6: This will cause the output of the ListingWindow to be on the screen again instead of using the file

 

Now you can use regular expressions, etc. to handle the *.txt file.

 

Hope that helps,

 

Bye,

 

Flo

Re: Export text from the Operation's information window

Valued Contributor
Valued Contributor
Thank you so much!