Cancel
Showing results for 
Search instead for 
Did you mean: 

Export to jt with correct file name

Phenom
Phenom

Hi,

I've the journal that export to jt. The jt file name have alwais tha '_'. It's possible to have the same jt file name as the original prt file name ?

For example 1-2345.prt -> 1-2345.jt and not 1_2345.jt

Thank you...

Using NX 11 / RuleDesigner PDM

1 REPLY

Re: Export to jt with correct file name

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I don't see anything in the journal code that would change the file name like that.

 

I suspect that in your JT config file, the "autoNameSanitize" option is set to true (or it is not set, in which case it defaults to 'true'); which is making the change.

https://docs.plm.automation.siemens.com/tdoc/nx/10/nx_help/#uid:index_nxtojt:xid487329:configuration...

 

https://docs.plm.automation.siemens.com/tdoc/nx/10/nx_help/#uid:xid487763