Cancel
Showing results for 
Search instead for 
Did you mean: 

Extracting result probe values from entire solution?

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hi

 

I'm trying to get back to NXOPEN and the goal now is to generate the information of result probe. 

The CAE.resultprobe.information does not return a value and It's not clear to me how to cycle through an entire list of result probes in a specific solution. 

 

Any help would be apprciated. 

 

6 REPLIES 6

Re: Extracting result probe values from entire solution?

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

https://community.plm.automation.siemens.com/t5/NX-Programming-Customization-Forum/Result-probe-plot...

 

Does the above discussion or solution helps your query? or Please be specific what you are trying to get from the info file.

Re: Extracting result probe values from entire solution?

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Thanks. 

 

I've seen this topic but I'm looking at something completely different. 

I have a model with hundreds of probes defined. I want to automtically go over the entire list of probes in the active solution and write it to a text file (that is no problem) in a format of PROBE_NAME,PROBE_INFORMATION.

 

Assume a PCB modeled with solid meshes and tons of compoenents, and now get all the results for that.. 

 

The next step would be to start generating probes based on polygon geometry name, but that is AFTER I get the post processing done. 

 

Re: Extracting result probe values from entire solution?

Phenom
Phenom

Do you have to use probe capability to do the result extraction you need?

Production: NX.CAE 10.0.2.6
Development: VB.NET (amateur level !)

Re: Extracting result probe values from entire solution?

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Currently, yes. 

I define a probe of maximum temperature over the polygon body which defines a componenet, and use that to extract the data, over many iterations or in steady state. 

 

There is no other real option for doing that, unless SC had some built-in similar tools. 

Re: Extracting result probe values from entire solution?

Siemens Creator Siemens Creator
Siemens Creator
Sub Main()

...

        probeName = "combinedX"
        formula = "(X(""PT2"")+DX(""PT2""))-(X(""PT1"")+DX(""PT1""))"
        Call CreateResultProbe(aSolution, probeName, loadCase, loadcaseindex, formula)
        value(0) = ResultProbeValue(workSimPart, probeName)

        probeName = "combinedY"
        formula = "(Y(""PT2"")+DY(""PT2""))-(Y(""PT1"")+DY(""PT1""))"
        Call CreateResultProbe(aSolution, probeName, loadCase, loadcaseindex, formula)
        value(1) = ResultProbeValue(workSimPart, probeName)

        probeName = "combinedZ"
        formula = "(Z(""PT2"")+DZ(""PT2""))-(Z(""PT1"")+DZ(""PT1""))"
        Call CreateResultProbe(aSolution, probeName, loadCase, loadcaseindex, formula)
        value(2) = ResultProbeValue(workSimPart, probeName)

...

End Sub

Sub CreateResultProbe(ByVal simSolution1 As CAE.SimSolution, ByVal probeName As String, ByVal loadcase As Integer, ByVal loadcaseindex As Integer, ByVal formaula As String)

        Dim simResultReference1 As CAE.SimResultReference = simSolution1.Find("Structural")
        Dim solutionResult1 As CAE.SolutionResult = theSession.ResultManager.CreateReferenceResult(simResultReference1)

        Dim nullCAEResultProbe As CAE.ResultProbe = Nothing
        Dim nXObject1 As NXObject = Nothing

        Dim resultProbeBuilder1 As CAE.ResultProbeBuilder = Nothing
        resultProbeBuilder1 = simSolution1.CreateResultProbeBuilder(nullCAEResultProbe)
        resultProbeBuilder1.ProbeName = probeName
        resultProbeBuilder1.Loadcase = loadcase
        resultProbeBuilder1.LoadcaseIndex = loadcaseindex
        resultProbeBuilder1.ModelSelectionType = CAE.ResultProbeBuilder.SelectionType.None
        resultProbeBuilder1.ResultReferenceType = CAE.SimResultReference.Type.Structural
        resultProbeBuilder1.Formula = formaula

        nXObject1 = resultProbeBuilder1.Commit()
        resultProbeBuilder1.Destroy()

End Sub

Function ResultProbeValue(ByVal workSimPart As CAE.SimPart, ByVal probeName As String)

        Dim value As Double = Nothing

        Dim fieldManager1 As Fields.FieldManager = workSimPart.FieldManager
        Dim resultProbe1 As CAE.ResultProbe = CType(fieldManager1.FindObject(probeName), CAE.ResultProbe)

        Dim expression1 As Expression = workSimPart.Expressions.Create("tempFd=fd(""" & probeName & """)")

        value = expression1.Value

        workSimPart.Expressions.Delete(expression1) 'Required

        Return value

End Function

Re: Extracting result probe values from entire solution?

Experimenter
Experimenter

Would this code work to extract a Result Probe value if it is only a single value?

 

I see the use of fields but, at least in the GUI, there is no way to save Result Probe Infromation to a field.