Cancel
Showing results for 
Search instead for 
Did you mean: 

Feature Callback function

Innovator
Innovator

Is there a way to call a function every time a feature is created in a part?

 

 

 

5 REPLIES 5

Re: Feature Callback function

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You would have to look in the log file to figure out what "button" creates the feature type.

Then in Menuscript add a "post" action to that button.

The tricky bit will be if you need to have this set ONLY in modeling.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Feature Callback function

Innovator
Innovator
Yikes....I honestly have no idea where to go with that.
What would I even be looking for in the Log File?

Re: Feature Callback function

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Creating a block is (I think)

&MACRO MENU, 0, UG_MODELING_BLOCK_FEATURE UG_GATEWAY_MAIN_MENUBAR <rbn_modeling_home.rtb->rbn_feature.grb->rbn_feature_more.gly->RECENTLY_USED::rbn_feature_more.gly> ## ! 

UG_MODELING_BLOCK_FEATURE

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Feature Callback function

Innovator
Innovator
Goodness....well I will see what I can find. Thank you.

Re: Feature Callback function

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Menuscript is documented in the *API* documentation (not installed by default)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled