Cancel
Showing results for 
Search instead for 
Did you mean: 

File path for component insertion

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hello everyone!

 

I try to understand how do I control file path when I add components to assembly using NX Open. I can use an absolute path, but what about another option? Can I define search paths programmatically? Also, does 'from folder' option from the NX interactive makes sence in NX open?

1 REPLY

Re: File path for component insertion

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If you use the .OpenComponents method, the currently defined load options will be used. You can modify the load options programmatically as desired.