Cancel
Showing results for 
Search instead for 
Did you mean: 

Find Curves on a Specific Layer

Valued Contributor
Valued Contributor

Hello there,

 

I am trying to collect the curves on a certain layer with the following code:

 

Dim allCurves() As Curve = workPart.Curves.ToArray()
Dim curvesOnLayer(0) As Curve
Dim count As Integer
			
For Each cv As Curve In allCurves
    If cv.Layer = currentLayer Then
	ReDim Preserve curvesOnLayer(count)
	curvesOnLayer(count) = cv
	count += 1
    End If
Next

(currentLayer is defined somewhere else)

But it couldn't find any curves. I manually selected the features with the "Curve" selection intent on, and I could select them. So I am sure they are curve features.

 

I was wondering what is wrong with the code.

 

Thanks,

Kai

13 REPLIES

Re: Find Curves on a Specific Layer

Honored Contributor
Honored Contributor

In your code, what is the value of "currentLayer"? Are you sure that the curves that you are seeing reside on the layer that "currentLayer" represents?

Re: Find Curves on a Specific Layer

Valued Contributor
Valued Contributor

Thanks, cowski1.

 

Yes, I am sure about that.

Re: Find Curves on a Specific Layer

Honored Contributor
Honored Contributor

Try running this code to see if you get the same result (change the targetLayer value to your desired layer number before running the code):

 

Option Strict Off
Imports System
Imports System.Collections.Generic
Imports NXOpen
Imports NXOpen.UF

Module Module1

    Dim theSession As Session = Session.GetSession()
    Dim theUfSession As UFSession = UFSession.GetUFSession()

    Dim theUI As UI = UI.GetUI()
    Dim lw As ListingWindow = theSession.ListingWindow

    Sub Main()

        Dim markId1 As Session.UndoMarkId
        markId1 = theSession.SetUndoMark(Session.MarkVisibility.Visible, "find curves on layer")

        lw.Open()

        Dim curvesOnLayer As New List(Of Curve)
        Dim targetLayer As Integer = 1

        For Each tempCurve As Curve In theSession.Parts.Work.Curves
            If tempCurve.Layer = targetLayer Then
                curvesOnLayer.Add(tempCurve)
            End If
        Next

        lw.WriteLine(curvesOnLayer.Count.ToString & " curves found on layer: " & targetLayer.ToString)

        lw.Close()

    End Sub

    Public Function GetUnloadOption(ByVal dummy As String) As Integer

        'Unloads the image immediately after execution within NX
        GetUnloadOption = NXOpen.Session.LibraryUnloadOption.Immediately

    End Function

End Module

Re: Find Curves on a Specific Layer

Valued Contributor
Valued Contributor

Thanks, @cowski1. It still can't find the curves.

 

The file I am working on is an assembly. The curve is actually a linked composite curve in a component part. But I could select it as a curve manually.

 

Re: Find Curves on a Specific Layer

Honored Contributor
Honored Contributor

Can you post your test prt file?

Are you working in context of an assembly?

Re: Find Curves on a Specific Layer

Valued Contributor
Valued Contributor

The file I am working on is an assembly. The curve is actually a linked composite curve in a component part. But I could select it as a curve manually.

 

Capture.JPG

 

It is a large product file. I am sorry I cannot post it here.

Re: Find Curves on a Specific Layer

Honored Contributor
Honored Contributor

Is the curve linked from the component to the assembly or the other way around?

Which part is the work part when you run the journal?

Re: Find Curves on a Specific Layer

Valued Contributor
Valued Contributor

The curve is linked from the component to the assembly.

 

The workpart is the assembly.

Re: Find Curves on a Specific Layer

Honored Contributor
Honored Contributor

There must be something else going on in your assembly. I did a quick test; I created a line in the component and wave linked it to the assembly. The assembly is the display and work part, when running the code above, the linked line was found.