Cancel
Showing results for 
Search instead for 
Did you mean: 

Finding duplicate curves in a part

Innovator
Innovator

Is there a way to find duplicate curves in a given part.

What I mean is there a way programatically to find if there are any curves lying directly on top of each other?

1 REPLY

Re: Finding duplicate curves in a part

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

For the "simple" case, looking ONLY for IDENTICAL curves, compare endpoints and (as required for curve type) center or knot or whatever points.

 

For the more difficult case where curves partially overlap...you need to do more math.

 

Are these all "dumb" curves, NOT used for anything else?

Or are these curves used for other features (extrude/revolve/etc.)?  if this is the case, it will be more difficult to deal with.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled