Cancel
Showing results for 
Search instead for 
Did you mean: 

From Point TO Point operation to the related feature

Valued Contributor
Valued Contributor

Hello everyone,

 

I'm doing some analyzing about Point to Point operations.

I wanted to know if is it possible to reach from a Point to Point operation to the related features (Simple features that can be found by the FBM).

If is it may be possible, can someone advise me please, how can it be done and which API's should I look for?

 

Thanks in advance,

Tom.

3 REPLIES

Re: From Point TO Point operation to the related feature

Valued Contributor
Valued Contributor

Is there a way to extract the information from the "Specify Holes" field?

 

2016_08_08_14_26_32_Cycl_Def_205_Bohren_Pilot_A1_ANBOHREN_D16H7_A_90_B0_.png

 

Re: From Point TO Point operation to the related feature

If it is possible, it would be in GRIPNC. 

You would likely get the XZYIJK only.

Mark Rief
Retired Siemens

Re: From Point TO Point operation to the related feature

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

*if* you can get XYZIJK...

The only way I've thought of to get the modeling feature is to find the edge/arc with the same origin and (same or opposite) arc axis, then get the feature(s) associated to the edge, and then figure out (if more than 1) which one is the "hole"

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled