Cancel
Showing results for 
Search instead for 
Did you mean: 

GUI from a .dlx not displayed - Macro crahes with error

Gears Phenom Gears Phenom
Gears Phenom

To all,

 

I am playing with a Graphical User Interface (GUI) (created with the NX UI buildder) and the macro crashes when trying to display the GUI. I am getting the error msg

 

  Object reference not set to an instance of an object

 

and the lines of code "quoted" seem to point to the  Public Shared Sub Main() in the Public Class MyGUI

 

Ani idea what is not being initialised?

 

Thanks

 

Regards

 

JXB

Production: NX.CAE 9.0.3.4, NX.CAE 10.0.2.6
Development: VB.NET (amateur level !)
16 REPLIES

Re: GUI from a .dlx not displayed - Macro crahes with error

Siemens Phenom Siemens Phenom
Siemens Phenom

 

I think we'll need more information about what you are doing in order to help.  Can you post your code?  Are you running from the Journal interface, or are you building a .DLL?  What version of NX are you using?

 

Thanks!

Re: GUI from a .dlx not displayed - Macro crahes with error

Gears Phenom Gears Phenom
Gears Phenom

NX9. Runing from Play > Journal

Code cannot be posted at the moment but will look at replicating the problem

Production: NX.CAE 9.0.3.4, NX.CAE 10.0.2.6
Development: VB.NET (amateur level !)

Re: GUI from a .dlx not displayed - Macro crahes with error

Gears Phenom Gears Phenom
Gears Phenom

This is the Sub where the problem appears to be

 

    Public Shared Sub Main()
        Try
        	
            theNXMacroGUI = New NXMacroGUI()
            ' The following method shows the dialog immediately
            theNXMacroGUI.Show()
        
        Catch ex As Exception
        
            '---- Enter your exception handling code here -----
            theUI.NXMessageBox.Show("Block Styler", NXMessageBox.DialogType.Error, ex.ToString)
        Finally
		
            If theNXMacroGUI IsNot Nothing Then
                theNXMacroGUI.Dispose()
            End If
	
        End Try	
		
    End Sub

 

Production: NX.CAE 9.0.3.4, NX.CAE 10.0.2.6
Development: VB.NET (amateur level !)

Re: GUI from a .dlx not displayed - Macro crahes with error

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Is NX able to find the dlx file?

See the NX syslog for the information if it finds it.

 

The dlx file must be placed in an application subfolder of UGII_SITE_DIR, UGII_GROUP_DIR, UGII_USER_DIR or a folder containd in custom_dirs.dat

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: GUI from a .dlx not displayed - Macro crahes with error

Gears Phenom Gears Phenom
Gears Phenom

Thanks for the input Stephan.

 

I am not so sure about the importance of the .dlx file to be located in UGII_SITE_DIR, UGII_GROUP_DIR, UGII_USER_DIR or a folder containd in custom_dirs.dat

 

I have tested one of the provided example (CampbellCsvToAfu) and it works fine. ie the GUI is displayed. The function which seems to create the problem is "lifted" from this example

 

'   Instructions:
'   1) A copy of CampbellCsvToAfu.dlx must be in one of the following locations:
'        1.) In the same folder as CampbellCsvToAfu.vb
'        2.) From where NX session is launched
'        3.) $UGII_USER_DIR/application
'        4.) For released applications, using UGII_CUSTOM_DIRECTORY_FILE is highly
'            recommended. This variable is set to a full directory path to a file
'            containing a list of root directories for all custom applications.
'            e.g., UGII_CUSTOM_DIRECTORY_FILE=$UGII_ROOT_DIR\menus\custom_dirs.dat
'
'   2) Run this program from within a FEM or SIM file in NX Advanced Simulation
'      - Use 'Tools > Journal > Play' to run CampbellCsvToAfu.vb

 

Where do I get the NX syslog file?

 

Thanks

 

Regards

Production: NX.CAE 9.0.3.4, NX.CAE 10.0.2.6
Development: VB.NET (amateur level !)

Re: GUI from a .dlx not displayed - Macro crahes with error

Legend
Legend

If you run the (uncompiled) journal as you get it from the BlockStyler (dlx file in the same dir as vb file) the journal won't find the dlx file because the (compiled) journal.dll is located somewhere in the users temp dir. So you have to put the dlx file to one of the other locations suggested by the documentation.

But: with the default BlockStyler generated code you would get an other error message in this case (something like ...dlx file not found).

 

Regards

Jan

 

Jan Böttcher

Re: GUI from a .dlx not displayed - Macro crahes with error

Gears Phenom Gears Phenom
Gears Phenom

the NX example provided (see previous comment) does not need a .dll to run (and works fine!). I did have the issue of ".dlx file not found" initally and after going thorugh the example I fixed it (as per the example) using the following code (I replaced "CampbellCsvToAfu" by my own name !)

 

theDialogName = IO.Path.ChangeExtension(theSession.ExecutingJournal, "dlx")

If theDialogName = "" Then

  theDialogName = "CampbellCsvToAfu_BS.dlx"

Else

  If Not IO.File.Exists(theDialogName) Then
          theDialogName = "CampbellCsvToAfu.dlx"
   End If

End If

 

 

 

Production: NX.CAE 9.0.3.4, NX.CAE 10.0.2.6
Development: VB.NET (amateur level !)

Re: GUI from a .dlx not displayed - Macro crahes with error

Legend
Legend

I don't have the example 'CampbellCsvToAfu' in my NX installation. So I have to guess...

 

As for compiled/uncompiled: NX compiles your vb code on-the-fly when you start a journal, puts the result (named journal.dll) in the users temp dir and runs this compiled dll. Getting the journals name and path by theSession.ExecutingJournal gets you around the dll location problem.

 

I don't understand why you need the IF...THEN..ELSE clause but if your journal has the same name and path as your dlx file there seems to be nothing wrong with this part of your code and the error must be somewhere else.

 

Regards

Jan

 

 

 

 

Jan Böttcher

Re: GUI from a .dlx not displayed - Macro crahes with error

Gears Phenom Gears Phenom
Gears Phenom

attached is the zip file with the example if you are interested

Production: NX.CAE 9.0.3.4, NX.CAE 10.0.2.6
Development: VB.NET (amateur level !)