Cancel
Showing results for 
Search instead for 
Did you mean: 

Get RSEvent Excitation Function Name - How to?

Gears Phenom Gears Phenom
Gears Phenom

To all,

 

I am looking for the keyword to "extract" the name of the excitation function(s) associated with a Response Simulation Event, It seems that the .GetExcitations shoudl do the trick but 2 issues encountered; 

1. the variable type 'Excitation(') (or should it be 'CAE.Excitation()' ?) is not regonised,

2. I cannot see anything in the doc under 'Excitation' to get the name of the excitation function(s) (i.e the associated afu record) (NOT the name of the excitation itself).

 

Any idea?

 

Thanks

Regards

 

Dim theRespSimManager As NXOpen.CAE.ResponseSimulation.Manager = theSimPart.Simulation.ResponseSimulationManager	
Dim AllRespSimSolutions As CAE.ResponseSimulation.Solution() = theRespSimManager.Solutions.ToArray()
		
For Each myRespSimSol As CAE.ResponseSimulation.Solution In AllRespSimSolutions

	'theLW.WriteLine("solution name: " & myRespSimSol.GetSolutionName)
		
	For Each myRSEvent As CAE.ResponseSimulation.RSEvent In myRespSimSol.GetEvents()
		Dim theRSEventExcitation As CAE.Excitation = myRSEvent.GetExcitations()
	Next myRSEvent
	
Next myRespSimSol

 

Production: NX.CAE 9.0.3.4, NX.CAE 10.0.2.6
Development: VB.NET (amateur level !)
2 REPLIES

Re: Get RSEvent Excitation Function Name - How to?

Siemens Phenom Siemens Phenom
Siemens Phenom

This can be done, but it's not the most straightforward thing in the world to do. You need to go back through the builder for the particular type of excitation and retreive the information from the builder.

 

The attached example will list information for translational nodal excitations.

Re: Get RSEvent Excitation Function Name - How to?

Gears Phenom Gears Phenom
Gears Phenom

Thanks a lot for that JimB. I would never have got any of it even though I had started looking at the RSBuilder. 

 

Will look at the provided example with great interest.

 

Thanks again.  

Production: NX.CAE 9.0.3.4, NX.CAE 10.0.2.6
Development: VB.NET (amateur level !)