Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Get SymbolicThread associated to Hole

Gears Phenom Gears Phenom
Gears Phenom

In a block dialog I'm trying to get the user to select a Hole (feature type HolePackage) and from that I want to find the associated SymbolicThread for the Hole if there is one.

Initially I just thought I'd be able to do HolePackage.getChildFeatures(), but that returns nothing Man Indifferent

By hacking my code to interrogate the features in the part I found there is a feature which reports its type as SIMPLE_HOLE that is an internal feature (I guess internal to the HolePackage). It is this feature that has the SymbolicThread as a child.

Is there any way I can get the SIMPLE_HOLE from the HolePackage feature so I can then get the SymbolicThread? I can't seem to find any 'getInternalFeatures()' method...

Graham Inchley Snr R&D Engineer (Systems Development), Sandvik Coromant
Dell 7530 Precision, Win10, 32GB. Developing in: Java | C | KF
Production: [NX12.0.2 MP1]
5 REPLIES 5

Re: Get SymbolicThread associated to Hole

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Are you looking to get the actual arc objects that represent the simplified thread for a threaded hole? Or something else, like the thread data?

Re: Get SymbolicThread associated to Hole

Gears Phenom Gears Phenom
Gears Phenom

Nothing that complicated, I simply want to find the SymbolicThread Feature.

 

I found the following convoluted process works, but it's super clunky and I haven't yet tested if it only finds the SymbolicThreads associated to the Hole feature:

for each body associated to the hole
  for each face of the body
    if face is cylindrical
      for each feature associated to the face
        if feature is instance of BodyFeature
          for each child feature of BodyFeature
            if child feature is SymbolidThread
              collect child feature in a list
            end
          end
        end
      end
    end
  end
end

I was hoping to do something more like:

for each child feature of hole
  if child feature is SymbolidThread
     collect child feature in a list
  end
end

Or using Java Streams, a one liner:

List<SymbolicThread> threads = hole.getChildFeatures().filter(child -> child.featureType().equals("SYMBOLIC_THREAD")).collect(Collectors.toList());
Graham Inchley Snr R&D Engineer (Systems Development), Sandvik Coromant
Dell 7530 Precision, Win10, 32GB. Developing in: Java | C | KF
Production: [NX12.0.2 MP1]

Re: Get SymbolicThread associated to Hole

Gears Phenom Gears Phenom
Gears Phenom

The pseudo code I posted above with many 'for each' and 'if' statements did work, but found additional threads on the body if there were any. I've revised it now and got it to only find the thread for the hole feature I'm interested in.

From my original post you can see that I can find an 'internal' feature that reports it's type as SIMPLE_HOLE. This has the thread as a child. So it would be nice to be able to get the internal features of the main hole (type = HolePackage). Anyone know if its possible to get internal features? Obviously there is no simple 'Feature.getInternalFeatures()'.

Graham Inchley Snr R&D Engineer (Systems Development), Sandvik Coromant
Dell 7530 Precision, Win10, 32GB. Developing in: Java | C | KF
Production: [NX12.0.2 MP1]

Re: Get SymbolicThread associated to Hole

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I don't know of a direct way to get what you want, but I know that internal features will have the same timestamp as the 'external' feature. Iterating through the features, checking the timestamp, .IsInternal property, and feature type should get what you want.

 

The code in the link below loops through the feature tree and builds a dictionary for later reference. I have not done much work with internal features since this code was written, perhaps there is a better way to do it now.

https://community.plm.automation.siemens.com/t5/NX-Programming-Customization-Forum/Working-with-Hole...

Re: Get SymbolicThread associated to Hole

Gears Phenom Gears Phenom
Gears Phenom

Using the Timestamp, excellent idea!

I've now refactored my code to use this logic. For performance, rather than cycle through all features in the part, I decided to just cycle through the bodies that the Hole returns from .getBodies() and cycle through all features each of the bodies returns from .getFeatures().

Still would be nice to have a more robust way to find these things, but this solution is much better than mine.

Thanks @cowski1 .

Graham Inchley Snr R&D Engineer (Systems Development), Sandvik Coromant
Dell 7530 Precision, Win10, 32GB. Developing in: Java | C | KF
Production: [NX12.0.2 MP1]