Cancel
Showing results for 
Search instead for 
Did you mean: 

Get a geometry information of an object

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hello.

 

I use Python.

 

I need to get a geometry information of the Face as well as I get it through the user interface (Menu -> Information -> Object or Ctrl+I).

 

Actually I need just the following parameter:

 

Normal - Absolute    I  =   -0.420212290      
                     J  =   -0.907389507      
                     K  =   -0.008118760

 

I tried to record journal file:

 

selectedObjects1 = [NXOpen.NXObject.Null] * 1 
selectedObjects1[0] = face
self.theSession.Information.DisplayObjectsDetails(selectedObjects1)

 

But this code displays a ListingWindow. Of course I can parse it, but I think there is a better way.

 

How can I get this geometry parameter?

8 REPLIES

Re: Get a geometry information of an object

Honored Contributor
Honored Contributor

You can get some face information from the .AskFaceData function. If the face is planar, this will also give you the normal direction. If the face is not planar, the normal direction will change depending on where you measure it. Using the .AskFaceProps function, you can get the normal direction for a given U V parameter. Given a point in 3D space, you can get the U V parameter on the face with .AskFaceParm.

 

Some useful functions to get surface information:

  • AskFaceData
  • AskFaceProps
  • AskFaceUVMinMax
  • AskFaceParm

Re: Get a geometry information of an object

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Thank you! But I don't understand how to use it?

 

I found some information in official documentation here

 

 

Signature: AskFaceData(face)
Parameters: face (Tag) – Face obj_id

 

Ok. I wrote:

 

 

import NXOpen.UF
... k = NXOpen.UF.Modeling.AskFaceData(face.Tag) # face is an instance of NXOpen.Face

 

 

And I catch an error:

 

descriptor 'AskFaceData' requires a 'NXOpen.UF.Modeling' object but received a 'int'

 

Re: Get a geometry information of an object

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

I got it! I need to get session first:

 

theUfSession = NXOpen.UF.UFSession.GetUFSession()
jj = theUfSession.Modeling.AskFaceData(face.Tag)

Re: Get a geometry information of an object

Honored Contributor
Honored Contributor

There's a bit more to it than that. You'll want to consult the API help docs to get information on the required arguments to the AskFaceData function. The function returns several pieces of information; to do this, you must declare variables for it to operate on. The function will change the values of the variables that you pass in; after the function runs, the variables will hold the data corresponding to the face tag that you passed in.

The code below (in VB) shows how to call the function.

 

Dim faceType As Integer
Dim facePt(2) As Double
Dim faceDir(2) As Double
Dim bbox(5) As Double
Dim faceRadius As Double
Dim faceRadData As Double
Dim normDirection As Integer
theUfSession.Modl.AskFaceData(someface.tag, faceType, facePt, faceDir, bbox, faceRadius, faceRadData, normDirection)

 

A faceType value of 22 indicates that the surface is planar. If it is planar, the faceDir array will hold the normal direction.

Re: Get a geometry information of an object

Genius
Genius

here try this and let me know if it works. language is python

 

import NXOpen
import NXOpen.BlockStyler
import NXOpen.Features
import NXOpen.UF
import NXOpen.GeometricAnalysis
import NXOpen.Facet
import random
import math

class geom_info:
        # Constructor for NX Styler class
    # ------------------------------------------------------------------------------
    def __init__(self):
        
        # class members
        self.theSession = None
        self.theUI = None
        self.theLw= None
        self.theDialogName = ""
        self.theDialog = None
        #Get the UF session
        self.theUfSession = None

       

        try:
            self.theSession = NXOpen.Session.GetSession()
            self.theUI = NXOpen.UI.GetUI()
            self.theLw = self.theSession.ListingWindow #create print window
            self.theUfSession = NXOpen.UF.UFSession.GetUFSession() 
            
        except Exception as ex:
            # ---- Enter your exception handling code here -----
            raise ex
    
    def get_info(self):
# declare global variables
        global workPart, face_list
        self.theLw.Open()
        self.theLw.WriteLine("Hello NX World!")
        self.theLw.WriteLine("")
        workPart = self.theSession.Parts.Work
        theUfSession = NXOpen.UF.UFSession.GetUFSession()

        #get all the solid bodies
        for body in workPart.Bodies:
            
            #get a list of all the faces
            face_list=body.GetFaces()

        #cycle through each face in the solid body
        for i in range(len(face_list)):
            self.theLw.WriteLine(str(face_list[i]))

            #create a temp object
            temp_face=face_list[i]
            self.theLw.WriteLine("")
            #get the tag for each face
            self.theLw.WriteLine("The face tag is "+str(temp_face.Tag))
            self.theLw.WriteLine("")

            #A tuple consisting of (type,point,dir,box,radius,rad_data,norm_dir)
            jj = theUfSession.Modeling.AskFaceData(temp_face.Tag)
            self.theLw.WriteLine("Geometry info is "+str(jj))

            self.theLw.WriteLine("Face type is NX surface type code 16 = cylinder 17 = cone 18 = sphere 19 = revolved (toroidal) 20 = extruded 22 = bounded plane 23 = fillet (blend) 43 = b-surface 65 = offset surface 66 = foreign surface "+str(jj[0]))
            self.theLw.WriteLine("")
            self.theLw.WriteLine("Direction information is "+str(jj[0]))
            self.theLw.WriteLine("")
            self.theLw.WriteLine("Face Boundary is "+str(jj[1]))
            self.theLw.WriteLine("")
            self.theLw.WriteLine("Radius is "+str(jj[2]))
def main():
    try:

        #create instance of class
        myclass = geom_info()
#call the method
        myclass.get_info()
    except Exception as ex:
        # ---- Enter your exception handling code here -----
        NXOpen.UI.GetUI().NXMessageBox.Show("Block Styler", NXOpen.NXMessageBox.DialogType.Error, str(ex))
   
if __name__ == "__main__":
    main() 

 

Re: Get a geometry information of an object

Honored Contributor
Honored Contributor

@AntonAus,

Sorry, I missed that you were using Python; use @AlexLee's example instead...

 

@AlexLee,

Thanks for posting the example. I'd like to use Python more when we move to NX10, your example will come in handy.

 

When you write out the information, it looks like a few references are off... I think they should be:

            self.theLw.WriteLine("Direction information is "+str(jj[2]))
            self.theLw.WriteLine("")
            self.theLw.WriteLine("Face Boundary is "+str(jj[3]))
            self.theLw.WriteLine("")
            self.theLw.WriteLine("Radius is "+str(jj[4]))

Re: Get a geometry information of an object

Genius
Genius

Smiley Happy sure thing! One day I need to organize all my python code and create some examples/documentation.

Re: Get a geometry information of an object

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

You were right! This is Python. And AskFaceData returns me a tuple of values which are described in documentation. Now I completely understand how it works :-)

 

Thank you all!