Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Get displayed color

Experimenter
Experimenter

Hello everyone,

I currently have a program that changes line colors through DependentDisplay.ApplyWireframeEdit. however, when I run the program twice it must ignore the previous colored lines.

 

Every time I check the color of a line in DraftingCurve.color, only the original color is displayed.

 

Is there a way to identify the displayed color and not the original color?

 

Thank you very much.

1 REPLY 1

Re: Get displayed color

Siemens Legend Siemens Legend
Siemens Legend

The color of a DraftingCurve is defined by the Visible Lines setting of the member view or by a manual view dependent edit for that object and Information->Object reports the object color and the view dependent edits color.

 

You can get the VDE color with the C API function UF_VIEW_ask_vde_data

(or the UFView wrapper method like UFView.AskVdeData in NET).