cancel
Showing results for 
Search instead for 
Did you mean: 

Graficproblem with NX on Mac

Builder
Builder

Hi all,

 

we have a customer, who have performance problems with NX10 on a MacBook He told me that NX was very slow to rotate or move a model in the grafics-window.

 

Here are the technical data of the MacBook:

MacBook Pro 15 with Retina Display (2014-Model), bought in 2015.

OS X Yosemite Version 10.10.5

CPU : 2,8 GHz Intel Core I7 (4 Core )

16 GB 1600 MHz DDR3

Graficcards : Intel Iris Pro (Onboard) 1,6 GB dynamic (max.)  and Nvidia GeForce 750 M (PCIe) 2GB

Harddisc : 500GB SSD

 

Do anyone have experiance with such a divice? Are there known problemes with graficcards?

 

Michael

Michael Eichelberg, CAD-Consultant, Dr. Wallner Engineering Nord GmbH
Production: NX10.0.3 MP16, NX11.0.1 MP4
Development: Batch and VB Testing: NX12
1 REPLY

Re: Graficproblem with NX on Mac

Siemens Phenom Siemens Phenom
Siemens Phenom

 

I don't see either of those graphics adapters listed in the certification matrix.  You can see it if you go to this page:

 

http://www.plm.automation.siemens.com/en_us/support/gtac/

 

Click on Hardware and Software Certifications on the menu on the left, then on the page that appears, click on the link under the picture on the right, that says Hardware (Graphics Card) Certifications.