Cancel
Showing results for 
Search instead for 
Did you mean: 

Help with points

Innovator
Innovator

Is there a way to get the "point3d" position of your cursor, or when you click.

1 REPLY

Re: Help with points

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Many of the selection functions will return the position of the cursor at the time of the user's selection; see the .SelectTaggedObject method for one example. Also, there is the .SpecifyScreenPosition that allows the user to select a position in the graphics window.