cancel
Showing results for 
Search instead for 
Did you mean: 

How to create a point feature from the output of UF_UI_point_construct

Experimenter
Experimenter

Requirement :  I wanted to created an associative point feature by prompting the user to specify the point through UF_UI_point_construct.

 

The UF_UI_point_construct returns an smart point tag which I thought of using into the PointFeatureBuilder to create an associative feature in the part navigator but the builder throws an error saying "Associative to this object is not possible".

 

If I create this smart object through SO calls then pass to builder it works but I hard to find the difference between the smart object from UF_UI_point_construct and the SO calls.

 

Anyone has any idea?