Cancel
Showing results for 
Search instead for 
Did you mean: 

How to deploy multiple maintenance packs on several client PCs

Pioneer
Pioneer

I am 5 maintenance packs behind, maybe more on some machines, on installing these updates. Any suggestions on how to do this programmatically? I'm guessing there is some batch file code to do this? Also, does the most current pack contain everything that is in previous packs?

 

Thanks in advance for any help on this matter.

 

Ron

NX8.5.3.3

Windows 7(64-bit)

3 REPLIES

Re: How to deploy multiple maintenance packs on several client PCs

Honored Contributor
Honored Contributor

Install the latest maintenance release (MR), it includes all the updates to that point. Don't bother installing maintenance patches (packs?) (MP's) unless it addresses a specific problem that you are experiencing.

Re: How to deploy multiple maintenance packs on several client PCs

Esteemed Contributor
Esteemed Contributor

To answer your other question

MRs and MPs are cumulative

So MR3 includes everything from MR1 and MR2

And MR1 MP6 includes everything from MR1 MP1 thru MR1 MP6

 

So you only have to install the desired MR (and optionally one MP)

 

Ken

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP5 + patch/TC11.2
I'd rather be e-steemed than e-diseaseled


Re: How to deploy multiple maintenance packs on several client PCs

Esteemed Contributor
Esteemed Contributor

I am using WPKG to deploy software and I am executing run_ugsupdate.exe to install the MR or MP.

Make sure to change the command line switch from /p to /d in the INI-file for silent installation.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.0, FBM, MRL 3.1.4 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 10.1
Development: VB.NET, Tcl/Tk    Testing: NX12.0

How to Get the Most from Your Signature in the Community