Cancel
Showing results for 
Search instead for 
Did you mean: 

How to disable on-screen input boxes

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Many commands offer both an input in the command dialog box and an on-screen input box.

One user would like to jash use the cammand dialog and does not like the on-screen input.

F3 will hide both while you are working. That's great.

Is there a way to hide just the on-screen input and not the command dialog?

NX9

LMGi
www.TLMGi.com
1 REPLY 1

Re: How to disable on-screen input boxes

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Have you checked the customer defaults or user interface preferences?

 

If you don't find something there, then there is no way.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide