Cancel
Showing results for 
Search instead for 
Did you mean: 

How to get moment of inertia from Assembly and part file in NX through API

Creator
Creator
I have an part file that has two different entity(ExSmiley Surprisedne rectangle and one triangle).

I need  moment of inertia from Assembly and part file in NX through API.

Currentlythis is what i have tried.

Dim measureBodies2 As MeasureBodies
measureBodies2 = workPart.MeasureManager.NewMassProperties(massUnits2, 0.99, objects2)

 

But dont know API to get MOI from measureBodies2.

 

 

Please help me to get this .

 

Any help would be appreciated.

 

Thanks in advance.

1 REPLY

Re: How to get moment of inertia from Assembly and part file in NX through API

Siemens Phenom Siemens Phenom
Siemens Phenom

 

Sangeeta,

 

Good morning.  You can get that with the Open C call UF_MODL_ask_mass_props_3d.  This is also wrapped for use in .Net as UFModl.AskMassProps3d.

 

As with most of the wrapped calls, you need to see the details in the Open C Reference Guide.

 

This method provides a great deal of information in a large array of values:

 

double mass_props [ 47 ] Output Mass properties
[0] = Surface Area
[1] = Volume (0.0 For Thin Shell)
[2] = Mass
[3-5] = Center Of Mass (COFM), WCS
[6-8] = First Moments (centroidal)
[9-11] = Moments Of Inertia, WCS
[12-14] = Moments Of Inertia (centroidal)
[15] = Spherical Moment Of Inertia
[16-18] = Inertia Products, WCS
[19-21] = Inertia Products (centroidal)
[22-30] = Principal Axes, WCS
[31-33] = Principal Moments (centroidal)
[34-36] = Radii Of Gyration, WCS
[37-39] = Radii Of Gyration (centroidal)
[40] = Spherical Radius Of Gyration
[41-45] = Unused
[46] = Density

 

Note that these are relative to the WCS, rather than the absolute CSYS,which is a bit unusual in the API.

 

Best regards,

 

Steve