Cancel
Showing results for 
Search instead for 
Did you mean: 

How to pass the part as parameter to AskBoundingBoxExact ?

Creator
Creator

I want to create multiple boxes around all parts in an assembly, the example code shows that I can pass the selection as 

body.tag

to 

AskBoundingBoxExact

However, I would like to pass part instead of getting from the selection. 

 

I replaced 

a_body

with 

workPart.Bodies.Tag
displayPart.Bodies.Tag

but they do not work (errors return invalid parameter)

 

The working code with selection option

Option Strict Off
 
Imports System
 
Imports NXOpen
Imports NXOpen.UI
Imports NXOpen.Utilities
Imports NXOpen.UF
 
Module make_bounding_block_of_selected_body_relative_to_wcs
 
    Dim s As Session = Session.GetSession()
    Dim ufs As UFSession = UFSession.GetUFSession()
    Dim lw As ListingWindow = s.ListingWindow()
 
    Sub Main()
 
        Dim a_body As NXOpen.Tag = NXOpen.Tag.Null
        Dim csys As NXOpen.Tag = NXOpen.Tag.Null
        Dim target As NXOpen.Tag = NXOpen.Tag.Null
        Dim blockFeature As NXOpen.Tag = NXOpen.Tag.Null
 
        Dim min_corner(2) As Double
        Dim directions(2, 2) As Double
        Dim distances(2) As Double
        Dim edge_len(2) As String
 
        While select_a_body(a_body) = Selection.Response.Ok
 
            ufs.Csys.AskWcs(csys)
 
            ufs.Modl.AskBoundingBoxExact(a_body, csys, min_corner, directions, _
                distances)
 
            lw.Open()
 
            lw.WriteLine("Min_corner: " & _
                min_corner(0).ToString & ", " & _
                min_corner(1).ToString & ", " & _
                min_corner(2).ToString & ", ")
 
            lw.WriteLine("X direction: " & _
                directions(0, 0).ToString & ", " & _
                directions(0, 1).ToString & ", " & _
                directions(0, 2).ToString & ", ")
            lw.WriteLine("X distance: " & _
                distances(0).ToString)
 
            lw.WriteLine("Y direction: " & _
                directions(1, 0).ToString & ", " & _
                directions(1, 1).ToString & ", " & _
                directions(1, 2).ToString & ", ")
            lw.WriteLine("Y distance: " & _
                distances(1).ToString)
 
            lw.WriteLine("Z direction: " & _
                directions(2, 0).ToString & ", " & _
                directions(2, 1).ToString & ", " & _
                directions(2, 2).ToString & ", ")
            lw.WriteLine("Z distance: " & _
                distances(2).ToString)
 
            edge_len(0) = distances(0).ToString()
            edge_len(1) = distances(1).ToString()
            edge_len(2) = distances(2).ToString()
 
            ufs.Modl.CreateBlock(FeatureSigns.Nullsign, _
                                 target, min_corner, edge_len, blockFeature)
        End While
 
    End Sub
 
    Function select_a_body(ByRef a_body As NXOpen.Tag) As Selection.Response
 
        Dim message As String = "Select a body"
        Dim title As String = "Select a body"
        Dim scope As Integer = UFConstants.UF_UI_SEL_SCOPE_ANY_IN_ASSEMBLY
        Dim response As Integer
 
        Dim view As NXOpen.Tag
        Dim cursor(2) As Double
        Dim ip As UFUi.SelInitFnT = AddressOf body_init_proc
 
        ufs.Ui.LockUgAccess(UFConstants.UF_UI_FROM_CUSTOM)
 
        Try
            ufs.Ui.SelectWithSingleDialog(message, title, scope, ip, _
                         Nothing, response, a_body, cursor, view)
        Finally
            ufs.Ui.UnlockUgAccess(UFConstants.UF_UI_FROM_CUSTOM)
        End Try
 
        If response <> UFConstants.UF_UI_OBJECT_SELECTED And _
           response <> UFConstants.UF_UI_OBJECT_SELECTED_BY_NAME Then
            Return Selection.Response.Cancel
        Else
            ufs.Disp.SetHighlight(a_body, 0)
            Return Selection.Response.Ok
        End If
 
    End Function
 
    Function body_init_proc(ByVal select_ As IntPtr, _
                           ByVal userdata As IntPtr) As Integer
 
        Dim num_triples As Integer = 1
        Dim mask_triples(0) As UFUi.Mask
        mask_triples(0).object_type = UFConstants.UF_solid_type
        mask_triples(0).object_subtype = UFConstants.UF_solid_body_subtype
        mask_triples(0).solid_type = UFConstants.UF_UI_SEL_FEATURE_BODY
 
        ufs.Ui.SetSelMask(select_, _
                           UFUi.SelMaskAction.SelMaskClearAndEnableSpecific, _
                           num_triples, mask_triples)
        Return UFConstants.UF_UI_SEL_SUCCESS
 
    End Function
 
    Public Function GetUnloadOption(ByVal dummy As String) As Integer
 
        GetUnloadOption = UFConstants.UF_UNLOAD_IMMEDIATELY
 
    End Function

 

1 REPLY

Re: How to pass the part as parameter to AskBoundingBoxExact ?

Esteemed Contributor
Esteemed Contributor

A Body is not a Part.

A part can contain zero or more bodies

A rough outline is to

- find each part in the assembly

- for each part, find the displayed reference set

- for that reference set, get the body/bodies (if any)

- get the bounding box of each body.

 

Another option (???) might be to cycle thru the bodies in the assembly.  I think even if the body is in a component, you can still get the body in the assembly.

 

You'll have to figure out if the bounding box is in reference to component (0,0,0) or assembly zero/orientation.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP5 + patch/TC11.2
I'd rather be e-steemed than e-diseaseled