Cancel
Showing results for 
Search instead for 
Did you mean: 

How to quickly remove duplicated curves?

Valued Contributor
Valued Contributor

I have a part file with multiple curves but some of these curves are duplicated  (the ones in red have duplicated curves in blue) per attached picture and step file. How could I quickly remove them from the part file?

 

 Note: there may be more than 1 duplicated per curve

 

2017-06-06_19-33-06.png

2 REPLIES

Re: How to quickly remove duplicated curves?

Valued Contributor
Valued Contributor

Right now, I use the dictionary to hold the starting point and get rid of the duplicated but not sure if it is a really good way to do.

Re: How to quickly remove duplicated curves?

Legend
Legend
If they are all on the same plane you should be able to use optimize 2d curve.
Rob Newcomb, CAD/CNC/Simulation manager
Elmhirst Industries, Specializing in Prototype sheet metal stampings and assemblies

Production: NX 11.0.2.7 / Autoform r7 /WorkNC 2017 r2
Testing:NX12 EAP
PC: Rave Cadbeast: Intel(R) i7-4790K CPU @ 4.GHz /32gb ram /NVIDIA Quadro K2200 on Win10 Pro