Cancel
Showing results for 
Search instead for 
Did you mean: 

How to select Multiple Polygons Face in advanced simulation application using the Block UI Styler

Experimenter
Experimenter

Using the following post I am able to use the block styler to select a single polygon face.

 

Block UI Styler - How to select Polygon Face in advanced simulation application

 

It seems however that the BlockStyler.SelectObject method only allow the selection of a single polygon face.

 

Is there a way to select multiple faces?

 

2 REPLIES

Re: How to select Multiple Polygons Face in advanced simulation application using the Block UI Style

Siemens Phenom Siemens Phenom
Siemens Phenom

The SelectObject block has a "SelectMode" property that defaults to "Single". Set this property to "Multiple" to allow selection of more than one object.

 

https://docs.plm.automation.siemens.com/tdoc/nx/11/nx_api#uid:index_blockstyler:id1153911:id1154041:...

Re: How to select Multiple Polygons Face in advanced simulation application using the Block UI Style

Experimenter
Experimenter

Thanks,

 

Just tried it and it works fine.