Cancel
Showing results for 
Search instead for 
Did you mean: 

Icon Size in Blockstyler Dialogs

Legend
Legend

Icon size of icons in native NX dialogs can be customized by the Customize | Icons/Tooltips | Dialog Boxes settings.

Those settings seem to have no influence on the icon size of blockstyler generated Action Buttons.

Is there any way to have automatic icon sizes for blockstyler buttons or must I mimic the behaviour by using different bitmaps for different settings?

 

Regards,

Jan

Jan Böttcher
2 REPLIES

Re: Icon Size in Blockstyler Dialogs

I just checked NX 11 and it works fine:

styler_dialog_big_action_buttons.jpg

 

Are you sure your icons are specified with only the name? Nothing speicifying the size like sc or lc?

Mark Rief
Retired Siemens

Re: Icon Size in Blockstyler Dialogs

Legend
Legend

Hello Mark,

 

sorry for the delay. I was out of office for some time.

 

You are right. I specified the bitmap file with the whole path. Never thought that this may cause different behaviour since the block's docu states: "Any Valid bitmap image name as String (Full path can also be specified)"

 

Specifying only the bitmap name without path and extension results in the expected behaviour.

 

Regards,

Jan

 

 

Jan Böttcher