Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Implicit surfaces: cool stuff with Convergent Technology

Siemens Phenom Siemens Phenom
Siemens Phenom

Using Convergent Technology, it's easy to make some very interesting shapes defined by implicit surfaces. There's a presentation (movie and PDF file) on this topic here. There are applications in industrial design and 3D printing.

 

The code below was used to create the models shown in the presentation.

 

 

山田
yamada
2 REPLIES 2

Re: Implicit surfaces -- an application of Convergent Technology

Experimenter
Experimenter

Thank you very much!!! 

Re: Implicit surfaces -- an application of Convergent Technology

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

pretty cool stuff!

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled