Cancel
Showing results for 
Search instead for 
Did you mean: 

In Model dialog command populate to fill attribute first befor start work like in Drafting Populate.

Experimenter
Experimenter

Hi All,

 

Is there any possibiltiy that we can create a command or dailog box, whenever user create new component a dialog box will populate and ask to fill attribute first like always populate in drafting to fill title box values.

1 REPLY 1

Re: In Model dialog command populate to fill attribute first befor start work like in Drafting Popul

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Briefly, yes.

You will probably want o use Menuscript (see the API docs) and add a "post" action to the "File->New" button

You could add some filtering based on application (modeling, etc.)

If people don't answer here, you could have a moderator move this thread to the NX Programming & Customization forum...

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled