Cancel
Showing results for 
Search instead for 
Did you mean: 

Increase Raster Image Export Resolution

Experimenter
Experimenter

Is is possible to increase the resultion of a raster image export beyond the default? Right now it looks like the resolution is limited by the CGM input image (300 pixels/inch) that's used by NX to create the various other image formats (JPEG, TIFF, PNG).

 

Selecting higher resolution in the Plot menu only artifically increases the image resolution, but does not allow for higher resolution of curves (it just makes their lines thicker).

1 REPLY

Re: Increase Raster Image Export Resolution


Selecting higher resolution in the Plot menu only artifically increases the image resolution, but does not allow for higher resolution of curves (it just makes their lines thicker).


Did you mean the Print Dimension Resolution?

 

plot.PNG

 

Attached a document from GTAC which describe the process to export shaded image with different resolutions.

 

Ganesh Kadole, QA Analyst (PLM), SQS
Testing: NX 11 | NX 12 | TCIN
TC 11.2 | TC Vis 11.3 | AWC 3.2