Cancel
Showing results for 
Search instead for 
Did you mean: 

Initialising the RmsResultsEvaluationSettingBuilder ?

Gears Phenom Gears Phenom
Gears Phenom

To all

 

I have a small programme which creates rms results (stress or force) for a given list of event and list of groups. Program seems to work as intended but I have noticed the following problem. Consider the following steps done by the user;

 

  1. In a brand new NX session (start NX, open sim file). Assume everything is there in term of resp. simulation events, results, etc. It’s all “good”.
  2. Start the GUI for the programme
  3. Select groups, events and the result type
  4. Press ‘OK’ to start creating the results

While the programme loops (through the groups and events as intended) it does not manage to create the rms results requested HOWEVER If I manually create an rms result (say stress) the normal way (In NX) then re-do steps 2-4 described above then the program seems to work. In other words it does create the rms result requested.

 

It seems that by doing a “cold” start my programme lacks some initialisation. By doing at least 1 rms result the normal way, NX is somehow initializing something that is picked up by my programme.

 

I appreciate this is not an easy thing to explain, so I have put see the function I have created.

 

Does anyone know if "calls" to variables like

CAE.ResponseSimulation.PeakValueEvaluationSettingBuilder

 requires more than I have put?

 

Thanks
Regards

 

 

Function CreatePeakRMSResult(theRSEvent As CAE.ResponseSimulation.RSEvent, _
										stheEventType as String, _
										stheResQttyType As String, _
										stheRS2FilePath As String, _ 
										thearrFEElm() as CAE.FEElement) As Boolean
 
		Dim iError As Integer = 0
 
		Dim workSimPart As CAE.SimPart = CType(theSession.Parts.BaseWork, CAE.SimPart)
		Dim simSimulation1 As CAE.SimSimulation = workSimPart.Simulation()
 
		Dim peakValueEvaluationSettingBuilder1 As CAE.ResponseSimulation.PeakValueEvaluationSettingBuilder
		Dim peakValueEvaluationSetting1 As CAE.ResponseSimulation.PeakValueEvaluationSetting
 
		Dim rmsResultsEvaluationSettingBuilder1 As CAE.ResponseSimulation.RmsResultsEvaluationSettingBuilder
		Dim rmsResultsEvaluationSetting1 As CAE.ResponseSimulation.RmsResultsEvaluationSetting
 
		'Dim combinationEvaluationOptions1 As CAE.ResponseSimulation.CombinationEvaluationOptions
		Dim dataComponent1(3) As CAE.ResponseSimulation.DirectionDataComponent
			dataComponent1(0) = CAE.ResponseSimulation.DirectionDataComponent.X
			dataComponent1(1) = CAE.ResponseSimulation.DirectionDataComponent.Y
			dataComponent1(2) = CAE.ResponseSimulation.DirectionDataComponent.Z
			dataComponent1(3) = CAE.ResponseSimulation.DirectionDataComponent.Vonmises
 
		Dim nXObject1 As NXObject
 
		Dim sEventAndResType As String
 
		Try
 
			If stheEventType = "Transient" Then
 
				peakValueEvaluationSettingBuilder1 = simSimulation1.ResponseSimulationManager.EvaluationSettingManager. _
													CreatePeakValueEvaluationSettingBuilder(Nothing)
 
				'Variable to make reading of the code easier
				sEventAndResType = stheEventType & "-" & stheResQttyType
				If sEventAndResType = "Transient-Force" Then peakValueEvaluationSettingBuilder1.ResultType = CAE.ResponseSimulation.EvaluationResultType.ElementForce
				If sEventAndResType = "Transient-Stress" Then peakValueEvaluationSettingBuilder1.ResultType = CAE.ResponseSimulation.EvaluationResultType.Stress
 
				'combinationEvaluationOptions1 = peakValueEvaluationSettingBuilder1.CombinationOptions
				peakValueEvaluationSettingBuilder1.SetOutputElements(thearrFEElm)
				peakValueEvaluationSettingBuilder1.SetDataComponents(dataComponent1)
				'peakValueEvaluationSettingBuilder1.SetDescriptionString(description1)
				nXObject1 = peakValueEvaluationSettingBuilder1.Commit()
				peakValueEvaluationSetting1 = CType(nXObject1, CAE.ResponseSimulation.PeakValueEvaluationSetting)
				theSession.Post.UnloadResultFile(stheRS2FilePath)
 
				theRSEvent.EvaluatePeakValueResults(peakValueEvaluationSetting1)
 
				peakValueEvaluationSetting1.Destroy()
				peakValueEvaluationSettingBuilder1.Destroy()
 
			Else 'stheEventType = "Random"
 
				rmsResultsEvaluationSettingBuilder1 = simSimulation1.ResponseSimulationManager.EvaluationSettingManager. _
													CreateRmsResultsEvaluationSettingBuilder(Nothing)
 
				If sEventAndResType = "Random-Force" Then rmsResultsEvaluationSettingBuilder1.ResultType = CAE.ResponseSimulation.EvaluationResultType.ElementForce
				If sEventAndResType = "Random-Stress" Then rmsResultsEvaluationSettingBuilder1.ResultType = CAE.ResponseSimulation.EvaluationResultType.Stress
 
				'combinationEvaluationOptions1 = rmsResultsEvaluationSettingBuilder1.CombinationOptions
				rmsResultsEvaluationSettingBuilder1.SetOutputElements(thearrFEElm)
				rmsResultsEvaluationSettingBuilder1.SetDataComponents(dataComponent1)
				nXObject1 = rmsResultsEvaluationSettingBuilder1.Commit()
				rmsResultsEvaluationSetting1 = CType(nXObject1, CAE.ResponseSimulation.RmsResultsEvaluationSetting)
				theSession.Post.UnloadResultFile(stheRS2FilePath)
 
				theRSEvent.EvaluateRmsResults(rmsResultsEvaluationSetting1)
 
				rmsResultsEvaluationSetting1.Destroy()
				rmsResultsEvaluationSettingBuilder1.Destroy()
 
				CreatePeakRMSResult = True
 
			End if
 
		Catch ex As Exception
			'---- Enter your exception handling code here -----
			iError += 1
			CreatePeakRMSResult = False
			'Throw ex	
		End Try
 
	End Function

 

Production: NX.CAE 9.0.3.4, NX.CAE 10.0.2.6
Development: VB.NET (amateur level !)