Cancel
Showing results for 
Search instead for 
Did you mean: 

Input Box in NXOpen c++

Hi all,

 

I should need Input Box to take user values in NX 8.5 . I am using NXOpen c++, but not able to find method to input values through inputBox. How can I create InputBox using c++ code..

 

 

 

 

Thanks in advance

7 REPLIES

Re: Input Box in NXOpen c++

Valued Contributor
Valued Contributor

Well unfortunaley C++ does not have a standard GUI library. Microsoft never thought to optimize that method like they did with Visual Basic and C#. You will most likely have to build your form and use the Form.ShowMethod(). You can see more on that in the following link:

 

https://msdn.microsoft.com/en-us/library/c7ykbedk.aspx

 

Unless of course the NX comes pre-packaged with a GUI library for C++. I'm not sure. I think you will have to resort to using the above method.

Re: Input Box in NXOpen c++

Phenom
Phenom

You could try using the legacy C functions like uc1607(), uc1608(), uc1609() and uc1613().

See details here: UF_UI

Graham Inchley Snr R&D Engineer (Systems Development), Sandvik Coromant
Lenovo ThinkPad W540, Win7, 16GB. Developing in: Java | C | KF
Production: [NX8.5.3.3 MP11 64bit] Testing: [NX12.0.0.27 MP1]

Re: Input Box in NXOpen c++

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I'm not sure that it is available in C++, but the NXInputBox class might do the job.

Re: Input Box in NXOpen c++

Phenom
Phenom

I don't use C++. but I thought you could access all the old C stuff from there...

Graham Inchley Snr R&D Engineer (Systems Development), Sandvik Coromant
Lenovo ThinkPad W540, Win7, 16GB. Developing in: Java | C | KF
Production: [NX8.5.3.3 MP11 64bit] Testing: [NX12.0.0.27 MP1]

Re: Input Box in NXOpen c++

thank you junfan, using microsoft messagebox can solve my problem

Re: Input Box in NXOpen c++

Hello @Inch,

 

Can you give me any example how to use the legacy cfunctions uc1607....

Re: Input Box in NXOpen c++

Siemens Phenom Siemens Phenom
Siemens Phenom

 

If you search for uc1607 in the Solution Center, and then filter on the document type of nx_api, there are 72 example programs available that use that function.

 

You can add Open C into your Opdn C++ code, just be sure that you #include <uf_ui.h> - or whatever header is appropriate for the call you are using.