Showing results for 
Search instead for 
Do you mean 
Reply

Is there any way to find out the point object selected is of what form / type??

Hi,

 

Can any one let me know is there any way i can able to find out, whether or not from what option the point is selected from Block styler Select Object.

 

If i check the type of the object selected i will get only NXOpen.Feature.Point, but i would like to know the other SnapPointTypesEnabled options. i.e. if user selects a point, then whether or not that point is of ArcCenter Type or a Control Point or Existing Point or any other.

 

 

 

Thanks and Regards,

Maddy

Windows 7 x64
NX 8.5, NX 9.0. And also NX 7.5
Visual Studio 2010 SP1, 2012 Update 4
2 REPLIES

Re: Is there any way to find out the point object selected is of what form / type??

I have not tried this, but you might be able to get some information about where the point came from using:

 

theUfSession.So.AskParents(pointObj.Tag, UF_SO_ASK_ALL_PARENTS, numOfParent, parents)

Ric Hotchkiss
Applications Consultant
rhotchkiss@daasolutions.com

O: 860-749-3832x214
F: 860-749-3842
C: 860-463-8486
Design Automation Associates Inc
68 Bridge Street, Suffield CT 06078
Website: http://www.daassolutions.com

Engineering Software & Engineering Services:
Design Automation, Training & Mentoring
NX, Knowledge Fusion, NX/Open, Checkmate
Mechanical Design, Structural & Thermal Analysis

Re: Is there any way to find out the point object selected is of what form / type??

Hi, Guys 

 

Does anybody have an idea, how to find what type of point selected.?

 

Regards,

Maddy

Windows 7 x64
NX 8.5, NX 9.0. And also NX 7.5
Visual Studio 2010 SP1, 2012 Update 4