Cancel
Showing results for 
Search instead for 
Did you mean: 

Issue occurring during initializing the callback for created MenuButton in NX.

Creator
Creator

Hello All,

 

As mentioned in NX Documentation, I was creating the Menu in NX.

 

using the SampleNXOpenApplication.

C:\Program Files\Siemens\NX 9.0\UGOPEN\SampleNXOpenApplications\C++\MenuBarCppApp.

 

So following are the steps.

 

Step1 : I had added the Cpp & header file as mentioned in new Visual Studio Project.

Step2 : Created the Application & Startup directories in one of the drive,

             In Application folder i had addeD:

                     a. MenuBarCppApp.men
                     b. MenuBarCppApp.dll 
                     c. MenuBarCppApp.lib 
             In Startup
                    a. MenuBarCppAppButton.men

 

Step3 : Created a batch file to set NX Enviornment Variable directly (UGII_USER_DIR) I had attachted the content of batch file in txt file.

 

Step4 : Run the NX through Code & Selected New Model.

 

Sample Cpp Meun Button was created under Menu Tab(image 1Image1.png). I had added images for refrences

 

& after selecting one of the Tab(Print ID Button) getting an error msg.Image2.JPG

 

 

& had checked with the menu file too. The Names specified are similar to the names in the 

void CppMenuBarApplication::InitializeCallbacks() function.

 

Can anyone please help me ,where I  am going wrong.

 

Thanks

Rohit