Cancel
Showing results for 
Search instead for 
Did you mean: 

Jornal: Name of selected operation

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hello!

 

I'm struggling with journal for post processing selected operation with its name. So far it works for any operation, but I can't get variable of its name. I would be grateful for help.

 

Option Strict Off
Imports System
Imports NXOpen

Module NXJournal
Sub Main (ByVal args() As String)

Dim theSession As NXOpen.Session = NXOpen.Session.GetSession()
Dim workPart As NXOpen.Part = theSession.Parts.Work

Dim displayPart As NXOpen.Part = theSession.Parts.Display

' ----------------------------------------------
' Menu: Tools->Operation Navigator->Output->Postprocess...
' ----------------------------------------------
workPart.CAMSetup.OutputBallCenter = False

Dim objects1(0) As NXOpen.CAM.CAMObject
Dim theUI As UI = UI.GetUI()

objects1(0) = CType(theUI.SelectionManager.GetSelectedObject(0), NXOpen.CAM.Operation)
workPart.CAMSetup.PostprocessWithSetting(objects1, "WIRE_EDM_4_AXIS", "C:\~~\Desktop\12345.h", NXOpen.CAM.CAMSetup.OutputUnits.PostDefined, NXOpen.CAM.CAMSetup.PostprocessSettingsOutputWarning.PostDefined, NXOpen.CAM.CAMSetup.PostprocessSettingsReviewTool.PostDefined)

' ----------------------------------------------
' Menu: Tools->Journal->Stop Recording
' ----------------------------------------------

End Sub
End Module

 

Regards,

Sebastian

7 REPLIES

Re: Jornal: Name of selected operation

Genius
Genius

Hello Sebastian!

 

Dim curOperation As NXOpen.CAM.Operation
curOperation = CType(theUI.SelectionManager.GetSelectedObject(0), NXOpen.CAM.Operation)

You should now be able to get the name of the operation with

curOperation.Name

You are creating a variable called objects1(0) (Type: NXOpen.CAM.CAMObject), but

to get some properties of an operation you need a variable Type: NXOpen.CAM.Operation.

 

Hope that helps! Bye,

 

Flo

Re: Jornal: Name of selected operation

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Thank you Flo !

 

Now it works with one selected operation (vb file in attachment)

 

Is there any simple way to automate this, for example:

After selecting 10 operation journal will post process 10 files?

 

Regards,

Sebastian

Re: Jornal: Name of selected operation

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
For Each theSelectedObject as NXObject in theUI.SelectionManager.GetSelectedObjects()

    ' ... your code goes here with some modifications

Next

 

This is just out of my head, so you get a hint, the methods might be called differently.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Jornal: Name of selected operation

There are several vb examples that operate on the selected operations, or members of selected groups that are operations. Take a look in the install folder - UGOPEN\SampleNXOpenApplications\.NET\CAM for *OntSelection.vb.

Mark Rief
Retired Siemens

Re: Jornal: Name of selected operation

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Thank you for tip. After a few hours, journal is generating multiple files with different names of selected operation, but with same code inside it.

 

I can't link tagged operation in code below. I tried different ways but I failed. (Full code in annex)

 

'Check if the object is a operation
If TypeOf camObject Is CAM.Operation Then
'Get the current operation name
Dim CurrentName As String = camObject.Name()
Dim filepath As String = "C:\~~\Desktop"

'Post selected operation
Dim objects1(0) As NXOpen.CAM.CAMObject
Dim theUI As UI = UI.GetUI()
objects1(0) = CType(theUI.SelectionManager.GetSelectedObject(0), NXOpen.CAM.Operation)
workPart.CAMSetup.PostprocessWithSetting(objects1, "WIRE_EDM_4_AXIS", IO.Path.Combine(filepath, CurrentName & ".h") , NXOpen.CAM.CAMSetup.OutputUnits.PostDefined, NXOpen.CAM.CAMSetup.PostprocessSettingsOutputWarning.PostDefined, NXOpen.CAM.CAMSetup.PostprocessSettingsReviewTool.PostDefined)


End If

 

Regards,

Sebastian

Re: Jornal: Name of selected operation

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Replace

objects1(0) = CType(theUI.SelectionManager.GetSelectedObject(0), NXOpen.CAM.Operation)

with

objects1(0) = camObject

since

theUI.SelectionManager.GetSelectedObject(0)

will always use the first selected object and nothing else.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Jornal: Name of selected operation

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Thank you all! Works perfect!

 

Have a nice day!