Cancel
Showing results for 
Search instead for 
Did you mean: 

Journal Editor(Snap)--Troubleshooting

Pioneer
Pioneer

Hello,

 

I am new about using snap and using the NX journal editor and try to learn from the beginning,

 

I find a code which is very simple and which is in directory of [...NX 9.0]\UGOPEN\SNAP\Examples ,

 

The code is like this;

 

"Option Explicit Off
Imports Snap, Snap.Create

Module SnapSample
Sub Main()

 

InfoWindow.WriteLine("hello world")

 

End Sub
End Module"

 

but after click the "Play" icon

 

i get the error message which's name is "Journal Compile Errors" and in the message "Line 7:'Infowindow' is not declared. It may be inaccessible due to its protection level." is written...

 

after search this error message in the internet , i find some topics about this error message ;

 

*Missing references (Select the references [...NX] \ UGII \ managed )

*Broken References 

*Licensing Problems,

 

But i can't fix the problem ,  i can't find snap references etc.

 

Can anyone help me about this issue and give me some info about this error message; why it is happened and how i can fix it , what i need to do or arrange in the NX, to fix this error message.

 

Thanks....

 

 

 

 

6 REPLIES

Re: Journal Editor(Snap)--Troubleshooting

Siemens Phenom Siemens Phenom
Siemens Phenom

My guess is that you don't have a SNAP Author license. If I run the journal, I see the following in my syslog (note the 3rd last line: "Snap Author license found, adding reference to Snap.dll"):

 

&MACRO ASK_ITEM  1 (1 STRN 5707) = "D:\apps\Siemens\NX\9.0\UGOPEN\SNAP\Examples\GS Guide\Chapter 2\02_1_HelloWorld.vb"  !  
&MACRO FOCUS CHANGE IN 1
Using D:\apps\Siemens\NX\9.0\ugii\managed\ManagedLoader.dll to load managed DLL
Trying to load D:\apps\Siemens\NX\9.0\ugii\managed\ManagedLoader.dll
ManagedLoader.Load: D:\apps\Siemens\NX\9.0\ugii\managed\NXOpen.Utilities.dll Name:ctx://Journal5d1dc5f6
There are no context policies.

AppBase: D:\apps\Siemens\NX\9.0\ugii\managed\
Loaded assembly: NXOpen.Utilities, Version=4.0.0.0, Culture=neutral, PublicKeyToken=null from C:\Users\tsbernar\AppData\Local\assembly\dl3\L8C0KP80.RTV\2XBTMPXP.7AX\3746afa4\00255d24_68dfce01\NXOpen.Utilities.dll
Loaded assembly: System.Windows.Forms, Version=4.0.0.0, Culture=neutral, PublicKeyToken=b77a5c561934e089 from C:\windows\Microsoft.Net\assembly\GAC_MSIL\System.Windows.Forms\v4.0_4.0.0.0__b77a5c561934e089\System.Windows.Forms.dll
Loaded assembly: System.Drawing, Version=4.0.0.0, Culture=neutral, PublicKeyToken=b03f5f7f11d50a3a from C:\windows\Microsoft.Net\assembly\GAC_MSIL\System.Drawing\v4.0_4.0.0.0__b03f5f7f11d50a3a\System.Drawing.dll
Adding D:\apps\Siemens\NX\9.0\ugii\managed\\NXOpen.Utilities.dll as a reference item
Adding D:\apps\Siemens\NX\9.0\ugii\managed\\NXOpen.dll as a reference item
Adding D:\apps\Siemens\NX\9.0\ugii\managed\\NXOpen.UF.dll as a reference item
Adding D:\apps\Siemens\NX\9.0\ugii\managed\\MiniSnap.dll as a reference item
Evaluating whether to add Snap library: 
Snap Author license found, adding reference to Snap.dll 
Adding D:\apps\Siemens\NX\9.0\ugii\managed\\Snap.dll as a reference item
Adding D:\apps\Siemens\NX\9.0\ugii\managed\\NXOpenUI.dll as a reference item

Re: Journal Editor(Snap)--Troubleshooting

Siemens Phenom Siemens Phenom
Siemens Phenom

This exact scenario is covered in the SNAP Getting Started guide - for NX10, it is on page 114.

 

This is an excellent tutorial, and we suggest reading through it if you are getting started with SNAP, or even if you are getting started with NXOpen - there is a wealth of foundational material that will help you with either.

 

You can try using MiniSnap.dll instead of Snap.dll.  It allows limited access to some basic SNAP functionality when you don't have a SNAP license.

Re: Journal Editor(Snap)--Troubleshooting

Siemens Phenom Siemens Phenom
Siemens Phenom

Yes, as Steve said, work through the tutorials in the first few chapters of the "Getting Started with SNAP" guide. It's written for people exactly like you  Smiley Happy

 

In particular, it tells you how to use "MiniSnap", in case you don't have a SNAP license.

 

Also, it has a "Troubleshooting" chapter which tells you the possible causes of various errors (including the one you ran into). And, if you just follow the tutorial, you probably won't run into any errors, anyway.

山田
yamada

Re: Journal Editor(Snap)--Troubleshooting

Pioneer
Pioneer

Hello ,

 

First of all, thanks everyone who answer my question because of their interset and advice....

 

I find the tutorial which you mentioned and do it step by step...

 

Still can't start the code , i think i don't have author license...

 

After run the code (i write the code visual study 2012), i get this error message fom nx, below error message isn't mentioned in the tutorial so before decide to that "i have no author license for nx_snap", i want to be a sure....

 

hata-2.png

hata1.png

I also to check that if the problem is missing references or broken references, these two issue seems "OK"

So after this, Can i say that , i have no license for doing this??? So i need to use "MiniSnap", i want to be sure before decide....

hata-3.png

hata-4.png

Re: Journal Editor(Snap)--Troubleshooting

Siemens Phenom Siemens Phenom
Siemens Phenom

Take the first "Hello World" example from chapter 2 of the tutorial.

 

Change the second line of code from "Imports Snap, Snap.Create" to "Imports MiniSnap, MiniSnap.Create".

 

Run this code in the Journal Editor. If it works, then your problem is that you don't have a Snap Author license.

山田
yamada

Re: Journal Editor(Snap)--Troubleshooting

Experimenter
Experimenter

As you dont have SNAP autorised licence the error is showing. 

 

In the second line you should be replacing Snap with Minisnap.

Then try running code

 

for your refrence do as below.

Capture.PNG