Cancel
Showing results for 
Search instead for 
Did you mean: 

Link an point (in Test.prt file) in to a TableSection (drawing.prt file)

Pioneer
Pioneer

Hi,

 

Is there any way we can carry a link of an object in a tabular section.

 

For example, 

A point is present in Test.prt File and we need to link this point with the Table section available in a drawing file (Drawing1.prt).

Doesnot matter how, but is it possible to link this. So that from table i can open this part file.

 

if its not possible, could somebdoy is there any other alternative to have a link in tablesection for the point in Test.prt.

 

Regards,

Maddy

 

 

Windows 7 x64
NX 8.5, NX 9.0. And also NX 7.5
Visual Studio 2010 SP1, 2012 Update 4