Cancel
Showing results for 
Search instead for 
Did you mean: 

Looking for help/advice regarding how to access parasolid objects

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Code follows:
public static unsafe void DiagnTags(NXOpen.UF.UFSession ufsess, Body body)
    {
    // This call to AskKernelVersion(..) works ok
    NXOpen.UF.UFPs.KernelVersion psver = new NXOpen.UF.UFPs.KernelVersion();
    ufsess.Ps.AskKernelVersion(ref psver);
    GGG.Writev("", psver.build_number, psver.major_revision, psver.minor_revision, psver.year);

    Tag tagPS;
    PK.ENTITY_t pkent;
    PK.CLASS_t pkcls;
    foreach (Face faceIter in body.GetFaces())
        {
        ufsess.Ps.AskPsTagOfObject(faceIter.Tag, out tagPS);

        pkent = new PKENTITY((int)tagPS);
        PK.ERROR.code_t pkstatus = PK.ENTITY.ask_class(pkent, &pkcls);
        GGG.Write(pkstatus.ToString()); // pkstatus returns as modeller_not_started
        }
    }

The immediate problem is that my call to PK.ENTITY.ask_class(..) and many other methods fails returning modeller_not_started.

 

I have a parasolid development license, but perhaps there is something I must do to tell NX that I have that license.  Also the part that owns the body is sess.Parts.Work.

 

In an earlier effort that I cannot duplicate, I was getting past this call but value returned by ask_class indicated that the returned objects were not faces.  Once I get past the modeller_not_started issue, I will post that issue.

 

This posting relates to 2 other postings:
    "Trouble reading EDGE names"
    "Having difficulty reading parasolid attributes via NXOPEN."

3 REPLIES 3

Re: Looking for help/advice regarding how to access parasolid objects

Siemens Phenom Siemens Phenom
Siemens Phenom

Here is some code that I have used in the past:

 

      /// <summary>Get the Parasolid tag from this NX.Face</summary>
      internal NXOpen.Tag PsTag
      {
         get
         {
            NXOpen.Tag psTag;
            Globals.UFSession.Ps.AskPsTagOfObject(this.NXOpenTag, out psTag);
            return psTag;
         }
      }

      /// <summary>Get the Parasolid face from this NX.Face</summary>
      internal PK.FACE_t PsFace
      {
         get
         {
            PK.FACE_t psFace = (PK.FACE_t)(int)this.PsTag;
            return psFace;
         }
      }

 

I was calling the Parasolid .NET library, so I have

 

using PK = PLMComponents.Parasolid.PK_.Unsafe;

at the top of my C# file.

 

 

The code uses SNAP stuff (NX.Face, Globals.UFSession, etc) but the correspondence with NX/Open stuff should be obvious.

山田
yamada

Re: Looking for help/advice regarding how to access parasolid objects

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

The code I posted is also C# and equivalant to the code you offerred. 

 

Both approaches return a parasolid tag that looks like it might be valid. 

 

My troubles start after that point, when I try to do something with the parasolid tag.

 

In the code shown in the original posting I call 

pkstatus = PK.ENTITY.ask_class(pkent, &pkcls);

At the moment pkstatus returns as: modeller_not_started

and pkcls is @null.

Re: Looking for help/advice regarding how to access parasolid objects

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

I found the problem/solution

The pskernel.dll file should not have been copied to the startup folder with pskernel_net.dll.  Once I removed pskernel.dll the error (modeller_not_started) ceased and the class-type returned seems correct now.

 

When developing a free-standing parasolid application one always copies the 2 files together, but for integrating with NX we must use the one linked to NX.  The one I was using wasn't even the right version.