12-17-2014 08:06 AM
This may be the wrong place, feel free to point me elsewhere. Currently my group of 6 all are running stand alone NX10 is there a way to set it up where everyone and anyone who sits in design would pull a file in and all the heights and widths, note fonts, dimensions etc, “The Design Standards”……would be the same for everyone. Right now everyone has their own set up, so we have variation throughout the design room?
Thanks in advance
SRF
12-17-2014 09:36 AM
If you were on NX9, I'd suggest downloading the latest version of the "Rob Cohon" custom environments:
Read thru the docs on how to set up.
Unfortunately, I don't think there is an NX10 version yet, so you may have to start with the NX9 and "adapt" for NX10.
Basically, these environments allow setting up and using an area on a shared network drive so everyone sees the same customizations, etc. They support both native mode and Teamcenter.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled