Cancel
Showing results for 
Search instead for 
Did you mean: 

Looping through results of a Response Simulation (event)?

Gears Phenom Gears Phenom
Gears Phenom

To all

 

I am currently to establish a way of looping through the results in a Response Simulation Event. The idea is to find the last result to extract specific data. In my test case the result I am after is

'Peak Result X'

---Peak Element Force_X

---Peak Element Force_Y

---Peak Element Force_Z

where X is the ID

 

I have a function, see below, which loops through the results for a Solution but I am struggling to modify it for a Response Simulation (and its events). As a starting point the response simulation (name) and the event (name) entered by the user are known and both exist.

 

any help or pointer would be grealty appreciated.

 

Thanks

 

Regards

 

Dim simulation As CAE.SimSimulation = theSimPart.Simulation()
Dim solution As CAE.SimSolution = simulation.ActiveSolution()
		
Dim results As CAE.Result = GetResults(solution2)
Dim nLoadCases As Integer = results.AskNumLoadcases()

        theLW.Open()
        theLW.WriteLine("" + "Solution [" + solution.Name + "] has " + nLoadCases.ToString + " LoadCases ")

        For iLoadCase As Integer = 0 To nLoadCases-1

            Dim nIterations As Integer = results.AskNumIterations(iLoadCase)

            theLW.WriteLine("   " + "LoadCase [" + iLoadCase.ToString + "] has " + nIterations.ToString + " Iterations ")

            For iIterations As Integer = 0 To nIterations-1
                Dim resultTypes() As CAE.Result.Type
                Dim resultTypeDescription() As String
                results.AskResultTypes(iLoadCase, iIterations, resultTypes, resultTypeDescription)
                Dim nTypes = resultTypes.Length

                theLW.WriteLine("      " + "Iteration [" + iIterations.ToString + "] has " + nTypes.ToString + " Result Types ")

                For iType As Integer = 0 To nTypes-1
                    theLW.WriteLine("         " + "result type [" + iType.ToString() + "]: " + resultTypeDescription(iType ))

                Next

            Next

        Next
Function GetResults(ByRef solution As CAE.SimSolution) As CAE.Result
 'Function GetResults(ByRef solution As CAE.ResponseSimulation.Solution) As CAE.Result

  

Function GetResults(ByRef solution As CAE.SimSolution) As CAE.Result

Dim results As CAE.Result = Nothing
Dim part As BasePart = theSession.Parts.BaseWork
Dim theResultManager As CAE.ResultManager = theSession.ResultManager()

        If (theResultManager Is Nothing) Then
            theNXMessageBox.Show("Test", NXMessageBox.DialogType.Error, "No valid ResultManager")
            Return Nothing
        End If

        Dim solresults As CAE.SolutionResult = Nothing

        Try

            solresults = theResultManager.CreateSolutionResult(solution)

        Catch ex As Exception
            Return Nothing
        End Try

        If (solresults Is Nothing) Then
            theNXMessageBox.Show("Test", NXMessageBox.DialogType.Error, "Could not Access Solution Results")
            Return Nothing
        End If

        results = CType(solresults, CAE.Result)

        Return results
  
    End Function 

 

  

 

Production: NX.CAE 9.0.3.4, NX.CAE 10.0.2.6
Development: VB.NET (amateur level !)
5 REPLIES

Re: Looping through results of a Response Simulation (event)?

Gears Phenom Gears Phenom
Gears Phenom

did a bit of reading and found that the resp. simulation results may have to be accessed using CreateResponseEventResult(RSEvent). I therefore need to pass the RSEvent As CAE.ResponseSimulation.RSEvent to the function GetResult()

 

1st test failed because I get an error message about the:

'solution2' not being declared. It may be innacessible due ot its pretecitn level'

 

'solution2' is definitly declared, see code below.

 

any idea why 'solution2' declaratin is creating such problem?

 

Thansk

Regards

 

Try	
			
  Dim solution2 As CAE.ResponseSimulation.Solution = CType(workSimPart.Simulation.ResponseSimulationManager.Solutions.FindObject(sRespSimSolName), CAE.ResponseSimulation.Solution)

Dim RSEvent2 As CAE.ResponseSimulation.RSEvent = CType(solution2.FindObject(sRSEventName), CAE.ResponseSimulation.RSEvent)

solution2.ActiveEvent = RSEvent2
				
peakValueEvaluationSetting1 = CType(nXObject1, CAE.ResponseSimulation.PeakValueEvaluationSetting)

theSession.Post.UnloadResultFile(pathRS2File)
RSEvent2.EvaluatePeakValueResults(peakValueEvaluationSetting1)

peakValueEvaluationSetting1.Destroy()peakValueEvaluationSettingBuilder1.Destroy()
					
			
	Catch ex As Exception
								iError += 1
	'---- Enter your exception handling code here -----
	'Throw ex
End Try

 

 

 

Production: NX.CAE 9.0.3.4, NX.CAE 10.0.2.6
Development: VB.NET (amateur level !)

Re: Looping through results of a Response Simulation (event)?

Gears Phenom Gears Phenom
Gears Phenom
not sure why the original variable declaration didn't work but I slightly modified the code by defining the variables

Dim theActiveRespSim As CAE.ResponseSimulation.Solution
Dim theActiveRSEvent As CAE.ResponseSimulation.RSEvent

just before the Try ...Catch loop and it seems to work !

Accessing the results in the Resp. sim. Event of interest was indeed via

theResultManager.CreateResponseEventResult(theRSEvent)

Regards
Production: NX.CAE 9.0.3.4, NX.CAE 10.0.2.6
Development: VB.NET (amateur level !)

Re: Looping through results of a Response Simulation (event)?

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

When you get a "It may be inaccessible due to its protection level" warning/error, it usually has to do with the "scope" of the variable, which is determined by where it is declared. In your specific case, the variable is declared within the "Try" portion of the Try Catch block. The "lifetime" of the variable ends when the Try portion of the block ends; the variable will only be available to your program within the Try block. There are good reasons to limit the scope of variables like this; it is best practice to only use variables as long as needed and no longer within the program (this will avoid other code changing the value of your variables when you are not looking!).

 

I see from your most recent message that you moved the declaration of the variable outside of the Try block. The variable will now have a "scope" defined by the new container (sub/function, block, class, etc).

Re: Looping through results of a Response Simulation (event)?

Gears Phenom Gears Phenom
Gears Phenom

Thanks foe the clarification cowski1. Much appreciated.

 

Do you know if there is a option 'List Results'? There is nothing obvious in the doc (Results section).If one has a (peak) result in an NX response simulation, by right-clicking one gets the info on that result, see example below;

 

============================================================

Information listing created by : a.guy

Date : 14/04/2015 00:00:00

Current work part : C:\mytest_createpeak.sim

Node name : abcd123456

============================================================

Peak Element Force_X:

Coordinate System: Elemental

Unit: mN

--------------- Scalar

Elem 11:

Node 325133: 5.996e+005

Node 320704: -5.996e+005

Elem 12:

Node 325134: 3.813e+005

Node 320705: -3.813e+005

 

As I now have a programme which can create the results required and can loop through the results, I'd like to "list the results" and then using the listing window write to file (and window): 

 

theLW.SelectDevice(ListingWindow.DeviceType.FileAndWindow, outputTxTFile)

 

Thanks

 

Regards

Production: NX.CAE 9.0.3.4, NX.CAE 10.0.2.6
Development: VB.NET (amateur level !)

Re: Looping through results of a Response Simulation (event)?

Gears Phenom Gears Phenom
Gears Phenom

I vaguely rembered askign a very simialr question (about the 'List Results')

 

http://community.plm.automation.siemens.com/t5/NX-Programming-Customization/saving-info-window-data-...

 

and was pointed toward DisplayObjectsDetails(). Looking at the doc it seems that 'Result' is an NXObject

 

Has anyone a example on how to use DisplayObjectsDetails() ?

 

Thanks

 

Regards

 

 

 

Production: NX.CAE 9.0.3.4, NX.CAE 10.0.2.6
Development: VB.NET (amateur level !)