Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Macro Out of Sync

Legend
Legend

Hello,

 

I have a macro which causes a problem when another user is running it.

Does anyone know how I can fix this?

 

Thanks!

Regards,

Thomas

7 REPLIES 7

Re: Macro Out of Sync

Gears Phenom Gears Phenom
Gears Phenom

Macros are very dependant on everything being the same in the session.

  • Did the user start the macro from the same environment (Modelling, Drafting etc.)?
  • Is there anything different with the part open for the other user that would make different dialogs appear?

I would suggest taking the same steps interactively as the macro takes and watching what dialogs etc. appear. Compare these with what happens on a working set-up.

One recommendation is to always start a macro by going to Gateway. This means that no matter where a user starts the macro from it should work the same.

Graham Inchley Snr R&D Engineer (Systems Development), Sandvik Coromant
Dell 7530 Precision, Win10, 32GB. Developing in: Java | C | KF
Production: [NX12.0.2 MP1]

Re: Macro Out of Sync

Legend
Legend

Hi @Inch 

 

Thanks!!

 

  • Did the user start the macro from the same environment (Modelling, Drafting etc.)?
  • Yes the user starts the macro from the same environment. Modeling)
  • Is there anything different with the part open for the other user that would make different dialogs appear?
  • I don´t think so.

The problem seems to be when the macro tries to load the Drafting Preferences from the Customer Defaults.

When the user tries to do this step manually, everything works fine.

I had a look in the macro, because the message says that something is wrong in line 191.

 

I took a screenshot of that line.

Does this explain something to you why it is not working?

 

Best regards,

Thomas

Re: Macro Out of Sync

Gears Phenom Gears Phenom
Gears Phenom

Hi @TomK76 

Sorry, but trying to interpret why a macro is failing like that is really hard. The macro contents are not documented for us mere mortals, only Siemens would really be able to understand it.

Graham Inchley Snr R&D Engineer (Systems Development), Sandvik Coromant
Dell 7530 Precision, Win10, 32GB. Developing in: Java | C | KF
Production: [NX12.0.2 MP1]

Re: Macro Out of Sync

Legend
Legend

Hi @Inch 

 

no problem at all!

I´ll ask GTAC.

 

Thanks!

 

Thomas

Re: Macro Out of Sync

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Are both computers running the exact same version (major release and patch level) of NX? You can find the patch level by going into the help menu and picking system information (or something equivalent to that).

Re: Macro Out of Sync

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Or file -> help -> log file -> scroll down a bit, just after the "license information" section you should see something like:

 

For NX1851:

Main
NX 1851.2602
OM disk mark mode: 3

For NX10:

NX 10.0.3.5 MP19, 26Sep17.  See Maintenance Pack letter for detailed list of fixes.
NX 10.0.3.5
OM disk mark mode: 3
Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Macro Out of Sync

Legend
Legend

Hi @cowski1 

 

Yes there running on the exact same version.

 

But I took out the part of the macro that caused that problem.

 

So now it is working good for your needs!

 

Thanks!

 

Thomas